This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ISO7763-Q1:VCC1和 VCC2的电压电平不同

Guru**** 2811595 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1338128/iso7763-q1-different-voltage-level-for-vcc1-and-vcc2

器件型号:ISO7763-Q1

您好!

我是否可以为 VCC1和 VCC2使用不同的电压电平(例如、VCC1为5V、VCC2为3.3V)?

提前感谢。