This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ISO7721:VCC1=3.3V &放大器;VCC2=5V

Guru**** 2933120 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1399874/iso7721-vcc1-3-3v-vcc2-5v

器件型号:ISO7721

工具与软件:

尊敬的 Expert:

对于 ISO7221x、如果在应用中可以实现 VCC1=3.3V 和 VCC2 = 5V?