This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ISO6740-Q1:ISO6740-Q1

Guru**** 2928980 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1444135/iso6740-q1-iso6740-q1

器件型号:ISO6740-Q1

工具与软件:

如果 VCCx、特别是 VCC1为5V、那么 INx 是否为5V 电平、并在 VCC2为3.3V 的情况下执行到3.3V 输出的转换?