This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ISO6742:不同的 VCC 电压电平

Guru**** 2927950 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1449550/iso6742-different-vcc-voltage-levels

器件型号:ISO6742

工具与软件:

我们可以在 VCC1和 VCC2中使用不同的电压吗?例如:VCC1我想给5V DC 和 VCC2 3.3V DC。需要澄清一下。