This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74HCS595:Vcc 为3.3V 时的最大开关频率是多少?

Guru**** 2573535 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1517861/sn74hcs595-what-is-the-maximum-switching-frequency-when-vcc-is-3-3v

器件型号:SN74HCS595

工具/软件:

数据表仅列出了 Vcc 分别为2V、4.5V 和6V 时的最大开关频率、3.3V 时的最大开关频率是多少?