This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74LVC1G97:Vcc = 3.3V 时 Vt+最大值和 VT-min

Guru**** 2553450 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1070084/sn74lvc1g97-vt-max-and-vt--min-for-vcc-3-3v

部件号:SN74LVC1G97

对于 VCC = 3V Vt+最大值= 1.87V,VT-min = 0.84V。 VCC=3.3V 的 VT+最大值和 VT-最小 值是什么?