This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 查找数据速率为100Mbps的转换器TTL到LVCOMS25

Guru**** 2540720 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/603503/find-translator-ttl-to-lvcoms25-with-data-rate-100mbps

大家好,

我正在寻找一个能够将TTL (5V)转换 为LVCMOS25 (2.5V)的IC。
数据速率为100Mbps。
谁能指导我?
谢谢。