请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:SN74HC14 大家好,
根据我们的SN74HC14数据表,Vt+/Vt-数据 @ Vcc = 2V/4.5V/6V (DS的第5页),但 对于客户应用,Vcc实际上是3.3V,因此:
请您帮助评论SN74HC14的Vt+/Vt-(Vcc=3.3V),或者是否有一个公式?
谢谢和BR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.