This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74LV4T125:SPI中继器

Guru**** 2540720 points
Other Parts Discussed in Thread: SN74LV4T125, SN74LVC125A, SN74AHC367

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/667561/sn74lv4t125-spi-repeater

部件号:SN74LV4T125
主题中讨论的其它部件: SN74LVC125ASN74AHC367

尊敬的各位:

 我们的应用程序使用与40 cm 长距离CPU的SPI通信与其他器件,需要添加SPI中继器以保证正常通信,SN74LV4125是否可以用于 此 应用程序? 通信速率为50MHz, 输入电压为3.3V, Vcc也应为3.3V。

谢谢。