This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74HC541:SN74HC541

Guru**** 2540720 points
Other Parts Discussed in Thread: SN54LS174, SN74HC541

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1092985/sn74hc541-sn74hc541

部件号:SN74HC541
主题中讨论的其他部件:SN54LS174

使用NI Digital DAQ驱动具有TTL信号的D型触发SN74HC541PW。

我从SN74HC541PW获得了一个良好的信号,但当我将这些TTL信号应用到54LS174 (以PN JM3.851万/30106BEA出售3.0106万出售)时,没有输出。

SN54LS174芯片是现有设计的一部分,我必须按原状工作。输入D1-D6各连接一个0.1 UF电容器,此电容器连接到接地的50欧姆电阻器。

我想知道如何在这封邮件中包含pdf或JPG文件。 ~Hans