This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74LVC1G17:VT+范围

Guru**** 2537850 points
Other Parts Discussed in Thread: SN74LVC1G17

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/886974/sn74lvc1g17-vt-range

器件型号:SN74LVC1G17

 SN74LVC1G17数据表显示了在4.5V VC 下 VT+= 2.19~2.74V、在5.5V Vcc 下 VT+= 2.65~3.33V。

但现在该器件连接了5.0V 电源。

有人知道5.0V 时 Vt+的值范围是多少吗?