This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74HC74:如果输入电压介于低电平阈值和高电平阈值之间、输出状态将是什么?

Guru**** 2773145 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/899137/sn74hc74-what-will-the-output-status-if-the-input-voltage-is-between-low-level-and-high-level-threshold

器件型号:SN74HC74

如果使用 VCC=6V、低电平阈值为1.8V、高电平  阈值为4.2V。 如果输入电压介于1.8V 和4.2V 之间、该怎么办?