This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74LVTH125:用于驱动50 Ω 负载的并行缓冲器

Guru**** 2385750 points
Other Parts Discussed in Thread: SN74LVTH125
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/895046/sn74lvth125-parallel-buffers-to-drive-50-ohm-load

器件型号:SN74LVTH125

器件为 SN74LVTH125PW

缓冲器 IC 由3.3V 驱动、Iout 为32mA。 我能否将其中的两个缓冲器并联以增加驱动50欧姆负载(示波器输入)的输出电流?

32mA * 2个缓冲器= 64mA

64mA * 50 = 3.2V

有什么伤害吗?