This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74LVC1G07:当 Vcc = 3.3V 且 IOL = 4mA 或3.39mA 时、电压(最大值)是多少

Guru**** 2588655 points
Other Parts Discussed in Thread: SN74LVC1G07

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/960810/sn74lvc1g07-what-is-the-vol-max-when-vcc-3-3v-and-iol-4ma-or-3-39ma

器件型号:SN74LVC1G07

您好、先生、

当 Vcc 为3.3V、IOL 为4mA 或3.39mA 时、您能否帮助检查电压(最大值)是多少?

谢谢你。