This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74AHC125:要求不同电源提供输入电压

Guru**** 2845750 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1167754/sn74ahc125-ask-for-input-voltage-by-different-power-supply

器件型号:SN74AHC125

大家好、

数据表上的 Vcc 电源电压建议条件:最小2V、最大5.5V、输入电压:最小0V、最大5.5V

当我通过3.3V 电源电压使用 SN74AHC125PWR 时、我是否可以使用输入电压达到5V? 这意味着输入电压5V 将高于 Vcc 电源、这是否可行?

BRS

Hao