Other Parts Discussed in Thread: TXS0102
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TXS0102 您好、先生、
TXS0102是否是1.8V 至5V UART 电平转换器的合适解决方案、速度为 UART TX/RX 最大值3Mbps、UART 为推挽式?
谢谢你
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.