This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74LVC244A-Q1:3.3V 输入、1.8V 电源

Guru**** 2927270 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/838735/sn74lvc244a-q1-3-3v-input-with-1-8v-supply

器件型号:SN74LVC244A-Q1

大家好、

数据表提到、该器件可以在 VCC 3.3V 和5V 输入下运行、基本上可以在5V 至3.3V 之间进行电平转换。

该部件是否还可以在1.8V Vcc 和3.3V 输入下运行? 那么、要从3.3V 电平转换到1.8V 吗?

谢谢!

此致

Simon