Other Parts Discussed in Thread: TXB0104, LSF0108
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TXB0104 主题中讨论的其他器件: LSF0108
您好,
现在、客户需要 LVDS 电平转换来将1.8V 电平转换为3.3V 电平。 TI 的 TXB0104是否可以支持? 客户需求率大于70Mbps。可选择什么? 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.