This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74AVC4T234:我们使用 SN74AVC4T234进行时钟频率电平转换。

Guru**** 2874030 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1398618/sn74avc4t234-we-have-used-sn74avc4t234-for-clock-frequency-level-translation

器件型号:SN74AVC4T234

工具与软件:

大家好、团队成员:

 您能否确认以下电路将适用于从1.8V 到1.8V/3.3V 的100 MHz 时钟频率电平转换

  

请您确认以下电路将适用于从3.3V 到1.8V/3.3V 的100 MHz 时钟频率电平转换

此致、

Ganesh。 P