This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TXS0102:OE 引脚可以上拉至3.3V 而不是1.8V 吗?

Guru**** 2609895 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1450508/txs0102-can-the-oe-pin-pull-up-to-3-3-instead-of-1-8v

器件型号:TXS0102

工具与软件:

嗨、团队:

我是否可以知道 OE 引脚是否可以 上拉至3.3V、而不是1.8V?

谢谢!

Jayden