This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74LVC1G07:输入电压范围

Guru**** 2652675 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1476962/sn74lvc1g07-input-voltage-range

器件型号:SN74LVC1G07

工具与软件:

你(们)好

数据表显示 VI 为最大值6.5V。

当 VCC 电压为3V 时、最大6.5V (建议最大值5.5V)的输入电压范围是否有效?

谢谢~