请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他部件:DRV8303, DRV8307您好,
我使用的是24V - 48V和25A最大电流的集线器电机。该电流和电压的驱动器。请建议我使用一些电机驱动器控制器IC,它应该不可编程。
谢谢,顺祝商祺
Rohit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.