请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8601 尊敬的先生:
我们使用DRV8601 EVM,从PC线路输出进行连接。
当VDD=5.3V,
我修改了R1=100Kohm,您认为它将有2Vrms输出吗?
谢谢,Ian。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.