This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CCS/DRV8412DDWEVM:为什么每次关闭/打开电源后都要刷新DRV8412项目?

Guru**** 2350610 points
Other Parts Discussed in Thread: DRV8412
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/615634/ccs-drv8412ddwevm-why-do-i-flash-everytime-drv8412-project-after-power-off-on

部件号:DRV8412DDWEVM
主题中讨论的其他部件:DRV8412

工具/软件:Code Composer Studio

您好,

我正在使用带有步进电机的DRV8412 C2套件。 主板类型为REV G

使用示例GUI v9时,演示项目guI_project工作正常。

但是,每当我关闭/打开电源时,piccolo卡F2.8035万都不会启动,直到我再次刷新gui_project out文件。

我已将闪存项目设置为活动,而不是RAM。

我是否会错过正在进行的工作?