请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8818 您好,
我们的客户使用DRV8818,有疑问。
TI建议为充电泵使用0.22uF电容器。
是否可以并行使用两个0.1uF电容器而不是0.22uF?
客户希望使用与VM旁路电容器0.1uF相同的电容器。
此致,
Naoki Aoyama
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.