请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他部件:DRV8870, DRV8871, DRV8885好的,我们正在寻找驱动拉丝式直流电机(目前为24V,但可用于12V)。 电动机的电流最高可达800mA。 驱动器应具有内部电流控制。 是否有这样的TI驱动程序?
非常感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.