请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:LM4.858万 主题中讨论的其他部件:LM4.856万,,
大家好,
请帮助提供RL=1uF的输出电压与频率曲线。
现在我们重点关注4kHz。 在这种特性上,LM4.856万是否优于LM4.858万?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.