请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8805 主题中讨论的其他部件: DRV8806, DRV8804, DRV8846, DRV8884, DRV8803, TPL7407L
请帮助确认:drv8805或drv8806是否与客户马达匹配以替换sla7033。请帮助推荐更具成本效益的设备。
非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好 ,LI Iwan,
DRV8803,DRV8804,DRV8805和DRV8806可以驱动电机。 如果电动机以双极配置连接,也可以使用其它双极步进电动机驱动器,如DRV8846或DRV8884。
有几个关于应用程序的问题。
1)公共引脚处的电压是多少?
2)是否需要当前调节?
3)是否会使用齐纳来增加衰减?
4)是否在双极和选件中使用电机?
另一个选项是TPL7407L,尽管该设备没有DRV88xx设备的集成保护功能(过电流,短路CIRCUITR,欠压和带故障指示输出的过热)。