请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV1083-Q1 主题中讨论的其他部件:DRV1.0983万,
大家好,
我想知道我们是否可以监控DRV1.0983万的一些参数,以及在电动机负载未连接到IC时向MCU反馈。
因为客户开发了一个平台并驱动了4个电机,所以我提出了这个问题。 但在另一个项目中,他们希望使用相同的平台,仅驱动2个电机。 因此他们希望实现这种检测。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,
我想知道我们是否可以监控DRV1.0983万的一些参数,以及在电动机负载未连接到IC时向MCU反馈。
因为客户开发了一个平台并驱动了4个电机,所以我提出了这个问题。 但在另一个项目中,他们希望使用相同的平台,仅驱动2个电机。 因此他们希望实现这种检测。
谢谢!