请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DRV8885 您好,我的客户正在使用 DRV8885。我有一些问题。
对于电流跳变精度、意味着" IRREF = 1.0A、20%至63%电流设置、1%基准电阻、–12.5% 12.5%"
这是否意味着、例如、您设置了480mA 并实际测量了420mA-540mA?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.