请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DRV8885 在额定1.5A 电流下使用1.3A 时、运行是否有任何问题?
在数据表中、在非循环模式中描述了100%输出。
在1/2步进中、描述了71%设置。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.