请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DRV10987 drv10987能否以9000 rpm 的转速转动我的电机(24V、10极(5对)?
因为我看到最大速度是512
因此最大速度为51hz
因此、5对电机的最大转速 为612
我是对的吗?
谢谢"
利拉兹
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.