请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DRV2605 我们得到了 有关 drv2605的 PCN (PCN 编号:20180524001)。
CIVDD 发生了变化、值从0.1uF 变为1uF。
5年来、我们在当前设计中使用了0.1uF 电容。
我们是否应将其更改为1 μ F? 还是可以保持0.1 μ F?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.