请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DRV8908-Q1 团队好、我想问问、当 DRV8908处于睡眠模式时、以及当我唤醒器件时、通过 SPI 设置通信需要多长时间?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
团队好、我想问问、当 DRV8908处于睡眠模式时、以及当我唤醒器件时、通过 SPI 设置通信需要多长时间?