请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DRV2667EVM-CT 1)如何将 Anolog (IN+和 IN-)信号升压到0-120??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1)如何将 Anolog (IN+和 IN-)信号升压到0-120??
尊敬的 Soumyajit:
谢谢!
J·麦克弗森