This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DRV8912-Q1:器件之间的并行输出

Guru**** 2468460 points
Other Parts Discussed in Thread: DRV8144-Q1, DRV8912-Q1, DRV8143-Q1

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1275441/drv8912-q1-parallel-outputs-between-devices

器件型号:DRV8912-Q1
主题中讨论的其他器件: DRV8143-Q1和 DRV8144-Q1

您好!

我们能否将两个 DRV8912之间的输出并联到(1)具有更高的总体驱动电流(例如7A)、或(2)在驱动6A 时降低每个器件的温升(即每个 IC 承载约3A 电流)?