This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DRV2605:DRV2605不再驱动电机

Guru**** 2463330 points
Other Parts Discussed in Thread: DRV2605, DRV2605L

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1299272/drv2605-drv2605-no-longer-drives-motors

器件型号:DRV2605

在一个销售了数百个单元的项目中、我们偶尔会遇到配电板故障、出现电动机不再振动的症状。

我们已经进行了大量调查、最终得出结论:在某些情况下、DRV2605不再驱动电机!

当出现此问题时、我们可以保留微控制器、将不同的固件发回微控制器、我们可以观察到:

* DRV2605和微控制器之间的 I2C 通信正常

*我们可以发送 reset_dev 命令

*我们可以读取寄存器0并确认一切正常

*重新启动电机的唯一方法是切断电源至少1秒。 如果切断电源的持续时间小于此值、DRV2605将不会驱动电机。

 

DRV2605初始阶段如下所示:

* DRV2605_EN = 0

*延迟20ms

* DRV2605_EN = 1

*延迟2ms

*发送 RESET_DEV (DRV_MODE = 0x80)

*延迟20ms

*发送 CALIB (DRV_MODE = 0x07)

*查看附加文件中的校准

*发送 GO (DRV_MODE = 0x01)

*发送(DRV_MODE = 0x00)

 

振动阶段如下所示:

DRV_WRITE (DRV_GO、0x00);

DRV_WRITE (DRV_Waveform_SEQ_1、序列);

DRV_WRITE (DRV_GO、0x01);

电机是 LRA : https://www.digikey.fr/fr/products/detail/vybronics-inc/VG1040003D/10285886

您能帮助我们解释一下这个案例吗?

此致

DRV2605.h

/* Copyright 2018 ishtob
 * Driver for DRV2605L written for QMK
 *
 * This program is free software: you can redistribute it and/or modify
 * it under the terms of the GNU General Public License as published by
 * the Free Software Foundation, either version 2 of the License, or
 * (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program.  If not, see <www.gnu.org/.../>.
 */

#ifndef __DRV2605L_H
#define __DRV2605L_H

//#pragma once
#include "nrf_drv_twi.h"

/* Initialization settings

 * Feedback Control Settings */
#ifndef FB_ERM_LRA
#define FB_ERM_LRA 1 /* For ERM:0 or LRA:1*/
#endif
#ifndef FB_BRAKEFACTOR
#define FB_BRAKEFACTOR 3 /* For 1x:0, 2x:1, 3x:2, 4x:3, 6x:4, 8x:5, 16x:6, Disable Braking:7 */
#endif
#ifndef FB_LOOPGAIN
#define FB_LOOPGAIN 1 /* For  Low:0, Medium:1, High:2, Very High:3 */
#endif

#ifndef RATED_VOLTAGE
#define RATED_VOLTAGE 2 /* 2v as safe range in case device voltage is not set */
#ifndef V_PEAK
#define V_PEAK 2.8
#endif
#endif

/* LRA specific settings */
#if FB_ERM_LRA == 1
#ifndef V_RMS
#define V_RMS 2.5
#endif
#ifndef V_PEAK
#define V_PEAK 2.1
#endif
#ifndef F_LRA
#define F_LRA 205
#endif
#endif

/* Library Selection */
#ifndef LIB_SELECTION
#if FB_ERM_LRA == 1
#define LIB_SELECTION 6 /* For Empty:0' TS2200 library A to D:1-5, LRA Library: 6 */
#else
#define LIB_SELECTION 1
#endif
#endif

/* Control 1 register settings */
#ifndef DRIVE_TIME
#define DRIVE_TIME 25
#endif
#ifndef AC_COUPLE
#define AC_COUPLE 0
#endif
#ifndef STARTUP_BOOST
#define STARTUP_BOOST 1
#endif

/* Control 2 Settings */
#ifndef BIDIR_INPUT
#define BIDIR_INPUT 1
#endif
#ifndef BRAKE_STAB
#define BRAKE_STAB 1 /* Loopgain is reduced when braking is almost complete to improve stability */
#endif
#ifndef SAMPLE_TIME 
#define SAMPLE_TIME 3
#endif
#ifndef BLANKING_TIME
#define BLANKING_TIME 1
#endif
#ifndef IDISS_TIME
#define IDISS_TIME 1
#endif

/* Control 3 settings */
#ifndef NG_THRESH
#define NG_THRESH 2
#endif
#ifndef ERM_OPEN_LOOP
#define ERM_OPEN_LOOP 1
#endif
#ifndef SUPPLY_COMP_DIS
#define SUPPLY_COMP_DIS 0
#endif
#ifndef DATA_FORMAT_RTO
#define DATA_FORMAT_RTO 0
#endif
#ifndef LRA_DRIVE_MODE
#define LRA_DRIVE_MODE 0
#endif
#ifndef N_PWM_ANALOG
#define N_PWM_ANALOG 0
#endif
#ifndef LRA_OPEN_LOOP
#define LRA_OPEN_LOOP 0
#endif

/* Control 4 settings */
#ifndef ZC_DET_TIME
#define ZC_DET_TIME 0
#endif
#ifndef AUTO_CAL_TIME
#define AUTO_CAL_TIME 3
#endif

/* register defines -------------------------------------------------------- */
#define DRV2605L_BASE_ADDRESS       0x5A		/* DRV2605L Base address */
#define DRV_STATUS                  0x00
#define DRV_MODE                    0x01
#define DRV_RTP_INPUT               0x02
#define DRV_LIB_SELECTION           0x03
#define DRV_WAVEFORM_SEQ_1          0x04
#define DRV_WAVEFORM_SEQ_2          0x05
#define DRV_WAVEFORM_SEQ_3          0x06
#define DRV_WAVEFORM_SEQ_4          0x07
#define DRV_WAVEFORM_SEQ_5          0x08
#define DRV_WAVEFORM_SEQ_6          0x09
#define DRV_WAVEFORM_SEQ_7          0x0A
#define DRV_WAVEFORM_SEQ_8          0x0B
#define DRV_GO                      0x0C
#define DRV_OVERDRIVE_TIME_OFFSET   0x0D
#define DRV_SUSTAIN_TIME_OFFSET_P   0x0E
#define DRV_SUSTAIN_TIME_OFFSET_N   0x0F
#define DRV_BRAKE_TIME_OFFSET       0x10
#define DRV_AUDIO_2_VIBE_CTRL       0x11
#define DRV_AUDIO_2_VIBE_MIN_IN     0x12
#define DRV_AUDIO_2_VIBE_MAX_IN     0x13
#define DRV_AUDIO_2_VIBE_MIN_OUTDRV	0x14
#define DRV_AUDIO_2_VIBE_MAX_OUTDRV	0x15
#define DRV_RATED_VOLT              0x16
#define DRV_OVERDRIVE_CLAMP_VOLT    0x17
#define DRV_AUTO_CALIB_COMP_RESULT  0x18 
#define DRV_AUTO_CALIB_BEMF_RESULT  0x19
#define DRV_FEEDBACK_CTRL           0x1A
#define DRV_CTRL_1                  0x1B
#define DRV_CTRL_2                  0x1C
#define DRV_CTRL_3                  0x1D
#define DRV_CTRL_4                  0x1E
#define DRV_CTRL_5                  0x1F
#define DRV_OPEN_LOOP_PERIOD        0x20
#define DRV_VBAT_VOLT_MONITOR       0x21
#define DRV_LRA_RESONANCE_PERIOD    0x22

void drv2605l_twi_init (void);
void drv2605l_init(uint32_t powerPerCent);
void DRV_write(const uint8_t drv_register, const uint8_t settings);
uint8_t DRV_read(const uint8_t regaddress);
void drv2605l_pulse(const uint8_t sequence);

extern const nrf_drv_twi_t m_twi;


typedef enum DRV_EFFECT{
  clear_sequence      = 0,
  strong_click 		    = 1,
  strong_click_60 		= 2,
  strong_click_30 		= 3,
  sharp_click 		    = 4,
  sharp_click_60      = 5,
  sharp_click_30      = 6,
  soft_bump           = 7,
  soft_bump_60        = 8,
  soft_bump_30        = 9,
  dbl_click           = 10,
  dbl_click_60        = 11,
  trp_click           = 12,
  soft_fuzz           = 13,
  strong_buzz         = 14,
  alert_750ms         = 15,
  alert_1000ms        = 16,
  strong_click1       = 17,
  strong_click2_80    = 18,
  strong_click3_60    = 19,
  strong_click4_30    = 20,
  medium_click1       = 21,
  medium_click2_80    = 22,
  medium_click3_60    = 23,
  sharp_tick1         = 24,
  sharp_tick2_80      = 25,
  sharp_tick3_60      = 26,
  sh_dblclick_str     = 27,
  sh_dblclick_str_80  = 28,
  sh_dblclick_str_60  = 29,
  sh_dblclick_str_30  = 30,
  sh_dblclick_med     = 31,
  sh_dblclick_med_80  = 32,
  sh_dblclick_med_60  = 33,
  sh_dblsharp_tick    = 34,
  sh_dblsharp_tick_80 = 35,
  sh_dblsharp_tick_60 = 36,
  lg_dblclick_str     = 37,
  lg_dblclick_str_80  = 38,
  lg_dblclick_str_60  = 39,
  lg_dblclick_str_30  = 40,
  lg_dblclick_med     = 41,
  lg_dblclick_med_80  = 42,
  lg_dblclick_med_60  = 43,
  lg_dblsharp_tick    = 44,
  lg_dblsharp_tick_80 = 45,
  lg_dblsharp_tick_60 = 46,
  buzz 					= 47,
  buzz_80				= 48,
  buzz_60				= 49,
  buzz_40				= 50,
  buzz_20				= 51,
  pulsing_strong      = 52,
  pulsing_strong_80   = 53,
  pulsing_medium      = 54,
  pulsing_medium_80   = 55,
  pulsing_sharp       = 56,
  pulsing_sharp_80    = 57,
  transition_click		= 58,
  transition_click_80 = 59,
  transition_click_60	= 60,
  transition_click_40	= 61,
  transition_click_20	= 62,
  transition_click_10	= 63,
  transition_hum      = 64,
  transition_hum_80   = 65,
  transition_hum_60   = 66,
  transition_hum_40   = 67,
  transition_hum_20   = 68,
  transition_hum_10   = 69,
  transition_rampdown_long_smooth1  = 70,
  transition_rampdown_long_smooth2  = 71,
  transition_rampdown_med_smooth1   = 72,
  transition_rampdown_med_smooth2   = 73,
  transition_rampdown_short_smooth1 = 74,
  transition_rampdown_short_smooth2 = 75,
  transition_rampdown_long_sharp1   = 76,
  transition_rampdown_long_sharp2   = 77,
  transition_rampdown_med_sharp1    = 78,
  transition_rampdown_med_sharp2    = 79,
  transition_rampdown_short_sharp1  = 80,
  transition_rampdown_short_sharp2  = 81,
  transition_rampup_long_smooth1    = 82,
  transition_rampup_long_smooth2    = 83,
  transition_rampup_med_smooth1     = 84,
  transition_rampup_med_smooth2     = 85,
  transition_rampup_short_smooth1   = 86,
  transition_rampup_short_smooth2   = 87,
  transition_rampup_long_sharp1     = 88,
  transition_rampup_long_sharp2     = 89,
  transition_rampup_med_sharp1      = 90,
  transition_rampup_med_sharp2      = 91,
  transition_rampup_short_sharp1    = 92,
  transition_rampup_short_sharp2    = 93,
  transition_rampdown_long_smooth1_50  = 94,
  transition_rampdown_long_smooth2_50  = 95,
  transition_rampdown_med_smooth1_50   = 96,
  transition_rampdown_med_smooth2_50   = 97,
  transition_rampdown_short_smooth1_50 = 98,
  transition_rampdown_short_smooth2_50 = 99,
  transition_rampdown_long_sharp1_50   = 100,
  transition_rampdown_long_sharp2_50   = 101,
  transition_rampdown_med_sharp1_50    = 102,
  transition_rampdown_med_sharp2_50    = 103,
  transition_rampdown_short_sharp1_50  = 104,
  transition_rampdown_short_sharp2_50  = 105,
  transition_rampup_long_smooth1_50    = 106,
  transition_rampup_long_smooth2_50    = 107,
  transition_rampup_med_smooth1_50     = 108,
  transition_rampup_med_smooth2_50     = 109,
  transition_rampup_short_smooth1_50   = 110,
  transition_rampup_short_smooth2_50   = 111,
  transition_rampup_long_sharp1_50     = 112,
  transition_rampup_long_sharp2_50     = 113,
  transition_rampup_med_sharp1_50      = 114,
  transition_rampup_med_sharp2_50      = 115,
  transition_rampup_short_sharp1_50    = 116,
  transition_rampup_short_sharp2_50    = 117,
  long_buzz_for_programmatic_stopping  = 118,
  smooth_hum1_50 = 119,
  smooth_hum2_40 = 120,
  smooth_hum3_30 = 121,
  smooth_hum4_20 = 122,
  smooth_hum5_10 = 123,
} DRV_EFFECT;

/* Register bit array unions */

typedef union DRVREG_STATUS { /* register 0x00 */
  uint8_t Byte;
  struct {
    uint8_t OC_DETECT   :1; /* set to 1 when overcurrent event is detected */
    uint8_t OVER_TEMP   :1; /* set to 1 when device exceeds temp threshold */
    uint8_t FB_STS      :1; /* set to 1 when feedback controller has timed out */
    /* auto-calibration routine and diagnostic result
     * result  |  auto-calibation  |      diagnostic       |
     *   0     |      passed       | actuator func normal  |
     *   1     |      failed       | actuator func fault*  |
     * * actuator is not present or is shorted, timing out, or giving out–of-range back-EMF */
    uint8_t DIAG_RESULT :1;
    uint8_t             :1;
    uint8_t DEVICE_ID   :3; /* Device IDs 3: DRV2605  4: DRV2604  5: DRV2604L  6: DRV2605L */
  } Bits;
} DRVREG_STATUS;

typedef union DRVREG_MODE { /* register 0x01 */
  uint8_t Byte;
  struct {
    uint8_t MODE        :3; /* Mode setting */
    uint8_t             :3;
    uint8_t STANDBY     :1; /* 0:standby 1:ready */
  } Bits;
} DRVREG_MODE;

typedef union DRVREG_WAIT {
  uint8_t Byte;
  struct {
    uint8_t WAIT_MODE   :1; /* Set to 1 to interpret as wait for next 7 bits x10ms */
    uint8_t WAIT_TIME   :7;
  } Bits;
} DRVREG_WAIT;

typedef union DRVREG_FBR{ /* register 0x1A */
  uint8_t Byte;
  struct {
    uint8_t BEMF_GAIN    :2;
    uint8_t LOOP_GAIN    :2;
    uint8_t BRAKE_FACTOR :3;
    uint8_t ERM_LRA      :1;
  } Bits;
} DRVREG_FBR;

typedef union DRVREG_CTRL1{ /* register 0x1B */
  uint8_t Byte;
  struct {
    uint8_t C1_DRIVE_TIME    :5;
    uint8_t C1_AC_COUPLE     :1;
    uint8_t                  :1;
    uint8_t C1_STARTUP_BOOST :1;
  } Bits;
} DRVREG_CTRL1;

typedef union DRVREG_CTRL2{ /* register 0x1C */
  uint8_t Byte;
  struct {
    uint8_t C2_IDISS_TIME    :2;
    uint8_t C2_BLANKING_TIME :2;
    uint8_t C2_SAMPLE_TIME   :2;
    uint8_t C2_BRAKE_STAB    :1;
    uint8_t C2_BIDIR_INPUT   :1;
  } Bits;
} DRVREG_CTRL2;

typedef union DRVREG_CTRL3{ /* register 0x1D */
  uint8_t Byte;
  struct {
    uint8_t C3_LRA_OPEN_LOOP   :1;
    uint8_t C3_N_PWM_ANALOG    :1;
    uint8_t C3_LRA_DRIVE_MODE  :1;
    uint8_t C3_DATA_FORMAT_RTO :1;
    uint8_t C3_SUPPLY_COMP_DIS :1;
    uint8_t C3_ERM_OPEN_LOOP   :1;
    uint8_t C3_NG_THRESH       :2;
  } Bits;
} DRVREG_CTRL3;

typedef union DRVREG_CTRL4{ /* register 0x1E */
  uint8_t Byte;
  struct {
    uint8_t C4_OTP_PROGRAM     :1;
    uint8_t                    :1;
    uint8_t C4_OTP_STATUS      :1;
    uint8_t                    :1;
    uint8_t C4_AUTO_CAL_TIME   :2;
    uint8_t C4_ZC_DET_TIME     :2;
  } Bits;
} DRVREG_CTRL4;

typedef union DRVREG_CTRL5{ /* register 0x1F */
  uint8_t Byte;
  struct {
    uint8_t C5_IDISS_TIME         :2;
    uint8_t C5_BLANKING_TIME      :2;
    uint8_t C5_PLAYBACK_INTERVAL  :1;
    uint8_t C5_LRA_AUTO_OPEN_LOOP :1;
    uint8_t C5_AUTO_OL_CNT        :2;
  } Bits;
} DRVREG_CTRL5;

#endif

DRV2605.c

#include "nordic_common.h"
#include "nrf.h"
#include "ble_hci.h"
#include "ble_advdata.h"
#include "ble_advertising.h"
#include "ble_conn_params.h"
#include "nrf_sdh.h"
#include "nrf_sdh_soc.h"
#include "nrf_sdh_ble.h"
#include "nrf_ble_gatt.h"
#include "nrf_ble_qwr.h"
#include "app_timer.h"
#include "ble_nus.h"
#include "app_util_platform.h"
#include "bsp_btn_ble.h"
#include "nrf_pwr_mgmt.h"
#include "nrf_delay.h"
#include "nrf_drv_twi.h"
#include "nrf_log.h"

#include "DRV2605L.h"
#include <stdlib.h>
#include <stdio.h>
#include <math.h>

extern bool vibreurV2;

/* TWI instance ID. */
#if TWI0_ENABLED
#define TWI_INSTANCE_ID     0
#elif TWI1_ENABLED
#define TWI_INSTANCE_ID     1
#endif
/* TWI instance. */
const nrf_drv_twi_t m_twi = NRF_DRV_TWI_INSTANCE(TWI_INSTANCE_ID);

uint8_t DRV2605L_transfer_buffer[20];
uint8_t DRV2605L_tx_register[0];
uint8_t DRV2605L_read_buffer[0];
uint8_t DRV2605L_read_register;

void drv2605l_twi_init (void)
{
    ret_code_t err_code;

    nrf_drv_twi_config_t twi_config = {
       .scl                = SCL_PIN_V1,
       .sda                = SDA_PIN_V1,
       .frequency          = NRF_DRV_TWI_FREQ_100K,
       .interrupt_priority = APP_IRQ_PRIORITY_HIGH,
       .clear_bus_init     = true
    };
    if (vibreurV2)
    {
        twi_config.scl = SCL_PIN_V2;
        twi_config.sda = SDA_PIN_V2;
    }

    err_code = nrf_drv_twi_init(&m_twi, &twi_config, NULL, NULL);
    APP_ERROR_CHECK(err_code);

    nrf_drv_twi_enable(&m_twi);
}

void DRV_write(uint8_t drv_register, uint8_t settings) 
{
    ret_code_t err_code;

    DRV2605L_transfer_buffer[0] = drv_register;
    DRV2605L_transfer_buffer[1] = settings;
    err_code = nrf_drv_twi_tx(&m_twi, DRV2605L_BASE_ADDRESS, DRV2605L_transfer_buffer, 2, false);
}

uint8_t DRV_read(uint8_t regaddress) 
{
    ret_code_t err_code;

    err_code = nrf_drv_twi_tx(&m_twi, DRV2605L_BASE_ADDRESS, DRV2605L_tx_register, 1, true);
 
    err_code = nrf_drv_twi_rx(&m_twi, DRV2605L_BASE_ADDRESS, DRV2605L_read_buffer, 1);
    DRV2605L_read_register = (uint8_t)DRV2605L_read_buffer[0];

    return DRV2605L_read_register;
}





void drv2605l_init(uint32_t powerPerCent)
{
    uint8_t tmp;

    drv2605l_twi_init();

    if (vibreurV2)
    {
        nrf_gpio_cfg_output(DRV2605_EN_V2);
        nrf_gpio_pin_write(DRV2605_EN_V2, 0);
    }
    else
    {
        nrf_gpio_cfg_output(DRV2605_EN_V1);
        nrf_gpio_pin_write(DRV2605_EN_V1, 0);
    }
    nrf_delay_ms(20);

    if (vibreurV2)
    {
        nrf_gpio_cfg_output(DRV2605_EN_V2);
        nrf_gpio_pin_write(DRV2605_EN_V2, 1);
    }
    else
    {
        nrf_gpio_cfg_output(DRV2605_EN_V1);
        nrf_gpio_pin_write(DRV2605_EN_V1, 1);
    }
    nrf_delay_ms(2);

    DRV2605L_transfer_buffer[0] = 0x06; //RESET
    nrf_drv_twi_tx(&m_twi, 0x00/*General call*/, DRV2605L_transfer_buffer, 1, false);

  //RESET_DEV
  DRV_write(DRV_MODE,0x80); 
  nrf_delay_ms(20);

  tmp = DRV_read(DRV_STATUS);
  NRF_LOG_INFO("drv2605: %02X", tmp);

  /* 0x07 sets DRV2605 into calibration mode */
  DRV_write(DRV_MODE,0x07); 

//  DRV_write(DRV_FEEDBACK_CTRL,0xB6);
    
  #if FB_ERM_LRA == 0
    /* ERM settings */
  DRV_write(DRV_RATED_VOLT, (RATED_VOLTAGE/21.33)*1000);
  #if ERM_OPEN_LOOP == 0
  DRV_write(DRV_OVERDRIVE_CLAMP_VOLT, (((V_PEAK*(DRIVE_TIME+BLANKING_TIME+IDISS_TIME))/0.02133)/(DRIVE_TIME-0.0003))); 
  #elif ERM_OPEN_LOOP == 1
  DRV_write(DRV_OVERDRIVE_CLAMP_VOLT, (V_PEAK/0.02196));
  #endif
  #elif FB_ERM_LRA == 1
  DRV_write(DRV_RATED_VOLT, (( (powerPerCent*V_RMS/100) * sqrt(1 - ((4 * ((150+(SAMPLE_TIME*50))*0.000001)) + 0.0003)* F_LRA)/0.02071)));
  #if LRA_OPEN_LOOP == 0
    DRV_write(DRV_OVERDRIVE_CLAMP_VOLT, ((V_PEAK/sqrt(1-(F_LRA*0.0008))/0.02133)));
  #elif LRA_OPEN_LOOP == 1
    DRV_write(DRV_OVERDRIVE_CLAMP_VOLT, (V_PEAK/0.02196));
  #endif
  #endif
      
  DRVREG_FBR FB_SET;
    FB_SET.Bits.ERM_LRA = FB_ERM_LRA;
    FB_SET.Bits.BRAKE_FACTOR = FB_BRAKEFACTOR;
    FB_SET.Bits.LOOP_GAIN =FB_LOOPGAIN;
    FB_SET.Bits.BEMF_GAIN = 0; /* auto-calibration populates this field*/
    DRV_write(DRV_FEEDBACK_CTRL, (uint8_t) FB_SET.Byte);
  DRVREG_CTRL1 C1_SET;
    C1_SET.Bits.C1_DRIVE_TIME = DRIVE_TIME;
    C1_SET.Bits.C1_AC_COUPLE = AC_COUPLE;
    C1_SET.Bits.C1_STARTUP_BOOST = STARTUP_BOOST;
    DRV_write(DRV_CTRL_1, (uint8_t) C1_SET.Byte);
  DRVREG_CTRL2 C2_SET;
    C2_SET.Bits.C2_BIDIR_INPUT = BIDIR_INPUT;
    C2_SET.Bits.C2_BRAKE_STAB = BRAKE_STAB;
    C2_SET.Bits.C2_SAMPLE_TIME = SAMPLE_TIME;
    C2_SET.Bits.C2_BLANKING_TIME = BLANKING_TIME;
    C2_SET.Bits.C2_IDISS_TIME = IDISS_TIME;
    DRV_write(DRV_CTRL_2, (uint8_t) C2_SET.Byte);
  DRVREG_CTRL3 C3_SET;
    C3_SET.Bits.C3_LRA_OPEN_LOOP = LRA_OPEN_LOOP;
    C3_SET.Bits.C3_N_PWM_ANALOG = N_PWM_ANALOG;
    C3_SET.Bits.C3_LRA_DRIVE_MODE = LRA_DRIVE_MODE;
    C3_SET.Bits.C3_DATA_FORMAT_RTO = DATA_FORMAT_RTO;
    C3_SET.Bits.C3_SUPPLY_COMP_DIS = SUPPLY_COMP_DIS;
    C3_SET.Bits.C3_ERM_OPEN_LOOP = ERM_OPEN_LOOP;
    C3_SET.Bits.C3_NG_THRESH = NG_THRESH;
    DRV_write(DRV_CTRL_3, (uint8_t) C3_SET.Byte);
  DRVREG_CTRL4 C4_SET;
    C4_SET.Bits.C4_ZC_DET_TIME = ZC_DET_TIME;
    C4_SET.Bits.C4_AUTO_CAL_TIME = AUTO_CAL_TIME;
    DRV_write(DRV_CTRL_4, (uint8_t) C4_SET.Byte);
  DRV_write(DRV_LIB_SELECTION,LIB_SELECTION);
  //start autocalibration
  DRV_write(DRV_GO, 0x01);

  /* 0x00 sets DRV2605 out of standby and to use internal trigger
   * 0x01 sets DRV2605 out of standby and to use external trigger */
  DRV_write(DRV_MODE,0x00); 
  
  /* 0x06: LRA library */
  DRV_write(DRV_WAVEFORM_SEQ_1, 0x01);

  /* 0xB9: LRA, 4x brake factor, medium gain, 7.5x back EMF
   * 0x39: ERM, 4x brake factor, medium gain, 1.365x back EMF */
  
  /* TODO: setup auto-calibration as part of initiation */

}

void drv2605l_pulse(uint8_t sequence)
{
  DRV_write(DRV_GO, 0x00);
  DRV_write(DRV_WAVEFORM_SEQ_1, sequence);
  DRV_write(DRV_GO, 0x01);
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    感谢您与我们联系。 您能否提供有关何时发现故障的详细信息? 当您尝试发送波形时、驱动器是否正常运行、然后停止工作?

    此致、
    悉尼诺斯卡特  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    不幸的是知道它何时停止工作客户打电话给"振动器不再工作"无法知道发送订单时是否发生故障或者是否是在电池轻微放电或其他任何情况

    但是真正观察到的是、当客户设备发回时、电池已充满系统中的其他所有设备都正常工作

    当我将示波器放在 SDA 和 SCL 引脚上时、将发送到 DRV2605的信号。

    微控制器重新启动时、我查询寄存器0x00、以确保 DRV2605正确响应、并且响应正确。

    但是、当我发送一个序列时、电机不会移动。

    如果我将电池短路(受保护)、主板会重新启动、但电机仍然不工作。

    另一方面,如果我取出电池1或2秒,板重新启动和振荡器完美的工作...

    我目前有500台设备在使用中、已在10台不同设备上发现大约10次问题。

    此致、

    盖坦

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    是否可以在取出电池之前探测电源引脚并在取出电池时截取屏幕截图?  电源可能需要一些时间才能完全变为0、这就是电池必须在最短时间内耗尽的原因。 如果在这些引脚为零之前放回电池、器件不会复位。  

    当您读取0x00时、您会读回什么内容? 该寄存器包含一些可能指向该问题的标志。  

    此外、当器件上电时、有一个250us 的启动序列、其中需要设置某些寄存器、这些操作需要在向器件发送任何写入操作之前完成。 由于速度太快、这可能不是您的问题、但最好仔细检查一下。

    希望这对您有所帮助!

    此致、
    悉尼诺斯卡特  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    很遗憾、我无法重现此问题、我每2个月就有大约1台设备出现此问题。

    提及 DR2605电源故障时、需要说明尽管出现在第19页的数据表中、DEV_RESET 命令似乎与 BOR 不同。

    当我读取寄存器0x00时、返回的值为0xE0。

    此致、

    盖坦

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    如果无法重现故障、就很难进行任何调试。 了解故障发生时间 和器件看到的情况等详细信息  对于解决问题至关重要、但我们可以解决 您在电路板上看到的问题。 如果您 找到 重现问题的方法、我们可以深入探究根本原因。  

    当复位完成后、DEV_RESET 寄存器应返回0、否则无法完成。 在您拉高该值后、它是否曾回到0?

    此致、
    悉尼诺斯卡特  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    确认 DEV_RESET 返回0。

    我的感觉是 DRV2605中有一个阶段只能因电源故障而复位。 因此、使用 DEV_RESET 不允许进行复位...

    此组件是否有勘误表?

    此致、

    盖坦

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    由于您正在从0x00读回0xE0、我假设您正在使用 DRV2605L、但希望进行仔细检查、因为您一直在说 DRV2605。  这些器件都没有勘误表。

    DRV2605L 有两种需要下电上电的状态:

    该器件有一个 I2C 看门狗计时器、可在4.33ms 无交互后复位通信、但该功能在待机状态下不可用、因此如果在该状态下丢失通信、必须对该器件进行下电上电以重新建立通信。 我认为、 如果在器件之前正常工作之后出现故障、这可能是根本原因。 (DRV2605L 数据表中的第8.3.11节)

    另一个 可能需要下电上电的原因是 Vdd 压摆率。 在 DRV2605L 数据表中、"如果 VDD 斜升速率低于3.6kV/s、则器件可能会进入未知状态。 在这种情况下、要恢复初始默认状态、器件必须以快于3.6kV/s 的 VDD 斜升速率进行下电上电。"    如果在上电后才发现问题、这可能是原因、因为压摆率可能接近该值并具有导致故障的变化。 ( DRV2605L 数据表中的第8.3.12.4节)

    此致、
    悉尼诺斯卡特