This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MCF8316A:速度环路精度

Guru**** 2430620 points
Other Parts Discussed in Thread: MCF8316A

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1409955/mcf8316a-speed-loop-accuracy

器件型号:MCF8316A

工具与软件:

您好!

我们如何理解数据表中的速度环路精度?

例如、MCF8316A 假设使用内部时钟时速度精度为3%、那么这是否意味着当速度为6000rpm 时、误差可能为6000+_180rpm?

我们是否有任何其他器件可以实现更高的精度?

谢谢!

Yishan Chen