This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DRV8316C:功率耗散图或者计算功率耗散的公式

Guru**** 2553450 points
Other Parts Discussed in Thread: DRV8316C

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1440707/drv8316c-power-dissipation-graph-or-formula-to-calculate-power-dissipation

器件型号:DRV8316C

工具与软件:

您好!

我查看了 DRV8316C 三相的数据表、但没有功率耗散图。 是否有功率耗散图或公式来计算功率耗散?

■验证环境
-电源电压: 12V
-工作温度:-20℃ 至50℃
-最大电机电流:5.8A/2秒
-稳态电流: 0.6A

谢谢!

Conor