大家好,团队
客户提出的问题可能需要您的帮助:
使用 eusci_a_UART_ex1_loopbackAdvanced 例程了解 MSP430FR2433的时钟,并在调试模式下暂停一段时间。 CS 模块的寄存器如下:
片段运行时钟 SMCLK = MCLK = BRCLK = DCOCLKDIV =~1MHz,ACLK = 32.768 kHz;即 DCO 用作 SMCLK 时钟源,SMCLK 用作波特率时钟源,但初始化时未配置 DCO。
但 DCOFFG 实际上显示了一个错误,不需要修复它?
main.c 中的代码如下:
/* --COPYRIGHT--,BSD * Copyright (c) 2016, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * --/COPYRIGHT--*/ //****************************************************************************** //! EUSCI_A0 External Loopback test using EUSCI_A_UART_init API //! //! Description: This demo connects TX to RX of the MSP430 UART //! The example code shows proper initialization of registers //! and interrupts to receive and transmit data. //! //! SMCLK = MCLK = BRCLK = DCOCLKDIV = ~1MHz, ACLK = 32.768kHz //! //! //! Tested on MSP430FR4133 //! ----------------- //! RST -| P1.0/UCA0TXD|----| //! | | | //! | | | //! | P1.1/UCA0RXD|----| //! | | //! //! This example uses the following peripherals and I/O signals. You must //! review these and change as needed for your own board: //! - UART peripheral //! - GPIO Port peripheral (for UART pins) //! - UCA0TXD //! - UCA0RXD //! //! This example uses the following interrupt handlers. To use this example //! in your own application you must add these interrupt handlers to your //! vector table. //! - USCI_A0_VECTOR. //****************************************************************************** #include "driverlib.h" uint16_t i; uint8_t RXData = 0, TXData = 0; uint8_t check = 0; uint32_t clockValue; void main(void) { // stop watchdog WDT_A_hold(WDT_A_BASE); // XT1 Setup //Set P4.1 and P4.2 as Function Input. /* * Select Port 4 * Set Pin 1, 2 to input Module Function, XT1. */ GPIO_setAsPeripheralModuleFunctionInputPin( GPIO_PORT_P2, GPIO_PIN0 + GPIO_PIN1, GPIO_PRIMARY_MODULE_FUNCTION ); //Set external clock frequency to 32.768 KHz CS_setExternalClockSource(32768); //Set ACLK=XT1 CS_initClockSignal(CS_ACLK,CS_XT1CLK_SELECT,CS_CLOCK_DIVIDER_1); //Start XT1 with no time out CS_turnOnXT1(CS_XT1_DRIVE_0); //Set SMCLK = DCO with frequency divider of 1 CS_initClockSignal(CS_SMCLK,CS_DCOCLKDIV_SELECT,CS_CLOCK_DIVIDER_1); //Set MCLK = DCO with frequency divider of 1 CS_initClockSignal(CS_MCLK,CS_DCOCLKDIV_SELECT,CS_CLOCK_DIVIDER_1); // Configure UART pins //Set P1.0 and P1.1 as Secondary Module Function Input. /* * Select Port 1 * Set Pin 0, 1 to input with function, (UCA0TXD/UCA0SIMO, UCA0RXD/UCA0SOMI). */ GPIO_setAsPeripheralModuleFunctionInputPin( GPIO_PORT_P1, GPIO_PIN4 + GPIO_PIN5, GPIO_PRIMARY_MODULE_FUNCTION ); /* * Disable the GPIO power-on default high-impedance mode to activate * previously configured port settings */ PMM_unlockLPM5(); //Configure UART //SMCLK = 1MHz, Baudrate = 115200 //UCBRx = 8, UCBRFx = 0, UCBRSx = 0xD6, UCOS16 = 0 EUSCI_A_UART_initParam param = {0}; param.selectClockSource = EUSCI_A_UART_CLOCKSOURCE_SMCLK; param.clockPrescalar = 8; param.firstModReg = 0; param.secondModReg = 0xD6; param.parity = EUSCI_A_UART_NO_PARITY; param.msborLsbFirst = EUSCI_A_UART_LSB_FIRST; param.numberofStopBits = EUSCI_A_UART_ONE_STOP_BIT; param.uartMode = EUSCI_A_UART_MODE; param.overSampling = EUSCI_A_UART_LOW_FREQUENCY_BAUDRATE_GENERATION; if(STATUS_FAIL == EUSCI_A_UART_init(EUSCI_A0_BASE, ¶m)) { return; } EUSCI_A_UART_enable(EUSCI_A0_BASE); EUSCI_A_UART_clearInterrupt(EUSCI_A0_BASE, EUSCI_A_UART_RECEIVE_INTERRUPT); // Enable USCI_A0 RX interrupt EUSCI_A_UART_enableInterrupt(EUSCI_A0_BASE, EUSCI_A_UART_RECEIVE_INTERRUPT); // Enable interrupt //Verify if the Clock settings are as expected clockValue = CS_getMCLK(); clockValue = CS_getACLK(); clockValue = CS_getSMCLK(); __enable_interrupt(); while(1) { TXData = TXData + 1; // Increment TX data // Load data onto buffer EUSCI_A_UART_transmitData(EUSCI_A0_BASE, TXData); while(check != 1) { ; } check = 0; } } //****************************************************************************** // //This is the USCI_A0 interrupt vector service routine. // //****************************************************************************** #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector=USCI_A0_VECTOR __interrupt #elif defined(__GNUC__) __attribute__((interrupt(USCI_A0_VECTOR))) #endif void EUSCI_A0_ISR(void) { switch(__even_in_range(UCA0IV,USCI_UART_UCTXCPTIFG)) { case USCI_NONE: break; case USCI_UART_UCRXIFG: RXData = EUSCI_A_UART_receiveData(EUSCI_A0_BASE); if(!(RXData == TXData)) // Check value { while(1) { ; } } check = 1; break; case USCI_UART_UCTXIFG: break; case USCI_UART_UCSTTIFG: break; case USCI_UART_UCTXCPTIFG: break; } }
请帮您检查此案例? 谢谢。
此致,
樱桃