This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR2355:LPM3电流高于预期

Guru**** 2516840 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1080910/msp430fr2355-lpm3-current-higher-than-expected

部件号:MSP430FR2355

尽管这似乎是一个常见问题,但迄今为止,解决办法尚未解决。

下面是设置。

微运行于外部10MHz 晶体。

CSCTL6将 XT1驱动器设置为最低功率。

ACLK 运行频率为10MHz/256 (39062.5HZ)

MCLK 和 SMCLK 以10MHz 运行。

一个计时器关闭 ACLK (用于唤醒微型)

一个计时器因高分辨率计时而关闭 SMCLK (当我们不睡觉时-在我们睡觉时更多)

DAC 和 SAC OA 打开。 OA 设置为低功耗模式

ADC 关闭

内部参考关闭(ADC (打开时)和 DAC 使用外部参考引用)。

CSCTL8具有 MOSCREQEN=0,SMCLKREQEN=0,MCLKREQEN=0和 ACKLREQEN=1。

CSCTL5,SMCLKOFF=0

要检查 LPM3静态电流,初始化已完成,全局中断将被关闭。 主要是,微执行 LPM3宏,它就位于 ACLK 与 TIMER0一起运行的位置。

总结一下,我认为我在 LPM3中运行了什么。

ACLK,39062.5 Hz

TIMER0以 ACLK 速率计时,中断关闭。

DAC 和 OA 开,(低功耗模式下典型为200uA)。

电源管理电路和内部调节器仍处于打开状态(默认设置)。

港口线路不会驱动任何负载。

因此,我希望 LPM3电流大约为200uA,加上这些其他微型部件使用的任何部件(我希望这种情况会很低)。  MCLK 和 SMCLK 应关闭。

但是,我的微安正在 LPM3中绘制325uA,这比预期的多大约100多微安。

我的初始化代码已附加。

有什么想法吗?

#include <msp430fr2355.h>



/*
 * functions.c
 *
 *  Created on: Dec 29, 2021
 *      Author: Engineering
 */

void InitSys(void)
{


    //**********************************
    // Clear LOCKLPM5 bit to enable GPIO
    //**********************************

    PM5CTL0 &= ~LOCKLPM5;   //


    //************************************
    // Configure I/O port lines
    // P1 first
    //
    // P1.0, Analog Input (A0), P10V_FB
    // P1.1, Analog Input (A1), SEC1
    // P1.2, Analog Input (A2), SEC2
    // P1.3, Digital Output, Unused
    // P1.4, Digital Output, Unused
    // P1.5, Digital Output, Unused
    // P1.6, Digital Output, Unused
    // P1.7, Digital Output, Unused
    //***********************************

    P1OUT = 0;
    P1DIR = 0b11111000;

    //***********************************
    // Configure alternate functions for
    // Port 1.
    //
    // P1.0 = A0 (Analog Input 0), 11
    // P1.1 = A1 (Analog Input 1), 11
    // P1.2 = A2 (Analog Input 2), 11
    // P1.5 = OA1O (Analog Output 1), 11
    //***********************************

    P1SEL0 = 0b00100111;
    P1SEL1 = 0b00100111;


    //***********************************
    // Configure Port2
    //
    // P2.0, Digital Output, Unused
    // P2.1, Digital Output, Unused
    // P2.2, Digital Output, Unused
    // P2.3, Digital Output, Unused
    // P2.4, Digital Output, Unused
    // P2.5, Digital Output, Unused
    // P2.6, XOUT, Do not care about DIR
    // P2.7, XIN, Do not care about DIR
    //************************************

    P2OUT = 0;
    P2DIR = 0b01111111;


    //***********************************
    // Configure P2.7 and P2.6 for
    // XIN and XOUT
    //***********************************

    P2SEL1 = 0b11000000;    // SEL1 for P2.7 and P2.6 are = 1, select XIN and XOUT respectively
    P2SEL0 = 0b00000000;    // SEL0 for P2.7 and P2.6 are = 0, select XIN and XOUT respectively


    //*************************************
    // Configure Port 3
    //
    // P3.0, Digital Output, Unused or MCLK
    // P3.1, Digital Output, Unused
    // P3.2, Digital Output, Unused
    // P3.3, Digital Output, Unused
    // P3.4, Digital Output, P10V_REG
    // P3.5, Digital Output, P10V_MEAS
    // P3.6, Digital Output, Unused
    // P3.7, Digital Output, Unused
    //*************************************

    P3OUT = 0;
    P3DIR = 0b11111111;

    //***********************************
    // Configure P3.0, MCLK Out
    //***********************************

    P3SEL1 = 0b00000000;    // SEL1 for P3.0 MCLK
    P3SEL0 = 0b00000001;    // SEL0 for P3.0 MCLK




    //*************************************
    // Configure Port 4
    //
    // P4.0, Digital Output, Unused
    // P4.1, Digital Output, Unused
    // P4.2, Digital Output, Unused
    // P4.3, Digital Output, Unused
    // P4.4, Digital Output, Unused
    // P4.5, Digital Output, Unused
    // P4.6, Digital Output, Unused
    // P4.7, Digital Output, Unused
    //**************************************

    P4OUT = 0;
    P4DIR = 0b11111111;



    //**************************************
    // Configure Port 5
    //
    // P5.0, Digital Output, Unused
    // P5.1, Digital Output, Unused
    // P5.2, Digital Output, Unused
    // P5.3, Digital Output, Unused
    // P5.4, Digital Output, Unused
    // P5.5 - P5.7 not available
    //**************************************

    P5OUT = 0;
    P5DIR = 0b00011111;



    //**************************************
    // Configure Port 6
    //
    // P6.0, Digital Output, AH
    // P6.1, Digital Output, AL
    // P6.2, Digital Output, BH
    // P6.3, Digital Output, BL
    // P6.4, Digital Output, Unused
    // P6.5, Digital Output, Unused
    // P6.6, Digital Output, Unused
    // P6.7, not available
    //**************************************

    P6OUT = 0;
    P6DIR = 0b01111111;


    //********************************
    // Initialize clocks
    // Use external xtal (10MHZ)
    // MCLK = 10 MHZ (10MHZ / 1)
    // ACLK = 39062.5 HZ (10MHZ / 256)
    // SMCLK = 10 MHZ (MCLK / 1), 10MHZ
    //*********************************

    //******************************************
    // CSCTL5
    // Bits 15-13 Reserved
    // Bit 12, VLOAUTOOFF = 0, VLO always on
    // Bits 11-9 Reserved
    // Bit 8, SMCLKOFF = 0, SMCLK On
    // Bit 7-6 Reserved
    // Bit 5:4, DIVS = 00, SMCLK = MCLK / 1
    // Bit 3 Reserved
    // Bits 2:1:0, DIVM = 000, MCLK = XT1CLK / 1
    //******************************************


    CSCTL5 = \
            DIVS_0 | \
            DIVM_0;


    //***********************************************************
    // Bits 15:14 Reserved
    // Bit 13, XT1FAULTOFF = 0, Enable switch from ACLK to REFO
    // Bit 12 Reserved
    // Bits 11:10:9:8 = 0101, Divide by XT1 by 256 for ACLK
    // Bit 7:6 = 00, Lowest crystal drive
    // Bit 5, XTS = 1, high frequency mode
    // Bit 4, XT1BYPASS = 0, XT1 sourced internally
    // Bits 3:2, XT1HFFREQ = 10, 6 to 16MHZ XTAL
    // Bit 1, XT1AGCOFF = 0, AGC ON
    // Bit 0, XT1AUTOOFF = 1, XT1 OFF WHEN NOT USED
    //************************************************************

    CSCTL6 = \
            DIVA__256 | \
            XT1DRIVE_0 | \
            XTS_1 | \
            XT1HFFREQ_2 | \
            XT1AUTOOFF_1_L;

    //*************************************************************
    // Bits 15:10 Reserved
    // Bits 9:8, SELA = 00, ACLK Source XT1CLK with divider
    // Bits 7-3 Reserved
    // Bits 2:1:0 = 010, MCLK and SMCLK source = XT1CLK
    //*************************************************************

    CSCTL4 = \
            SELA__XT1CLK | \
            SELMS__XT1CLK;


    //*************************************************************
    // CSCTL8
    // Bits 15:4 Reserved
    // Bit 3, MODOSCREQEN, 0=MODOSC conditional requests disabled
    // Bit 2, SMCLKRWQEN, 0=SMCLK conditional requests disabled
    // Bit 1, MCLKREQEN, 0=MCLK conditional requests disabled
    // Bit 0, ACLKEQEN, 1=ACLK conditional requests enabled
    //*************************************************************

    CSCTL8 = \
            MODOSCREQEN_0 | \
            SMCLKREQEN_0 | \
            MCLKREQEN_0 | \
            ACLKREQEN_1;



    //**************************************************
    // Configure ADC for following
    //
    // 12 bit operation
    //
    // ADCCLK source is SMCLK (10 MHZ)
    // ADCDIV = 3
    // ADCCLK = SMCLK / 3 = 3.33MHZ (max 4.4MHZ)
    //
    // Conversion time = (12 + 2) x 1/ADCCLK
    // Conversion time does not include sample and hold
    //
    // Select VSS as -VREF
    // Select VCC as +VREF
    //****************************************************

    //****************************************************
    // Bits 15-10 Reserved
    // Bits 9:8, ADCPDIV = 00, Pre-divide by 1
    // Bits 7:6 Reserved
    // Bits 5:4, ADCRES = 10, 12 bit conversion
    // Bit 3, ADCDF = 0, unsigned binary result
    // Bit 2, ADCSR = 1, ADC buffer set for 50ksps
    // Bit 1, Reserved
    // Bit 0, Reserved
    //****************************************************

    ADCCTL2 = \
            ADCPDIV_0 | \
            ADCRES_2 | \
            ADCSR;

    //****************************************************************
    // Bits 15:12 reserved
    // Bits 11:10, ADCSHS = 00, Sample and hold source is ADCSC bit
    // Bit 9, ADCSHP = 1, SAMPCON signal is sourced from sampling timer
    // Bit 8, ADCISSH = 0, sample input is not inverted
    // Bits 7:6:5, ADCDIV = 010, Divide source clock by 3 for ADCCLK
    // Bit 4:3, ADCSSEL = 10, SMCLK is ADCCLK source
    // Bits 2:1, ADCCONSEQ = 00, single channel conversion
    // Bit 0, ADCBUSY, Read only, 1=conversion active.
    //****************************************************************

    ADCCTL1 = \
            ADCSHS_0 | \
            ADCSHP_1 | \
            ADCISSH_0 | \
            ADCDIV_2 | \
            ADCSSEL_3 | \
            ADCCONSEQ_0;

    //******************************
    // Select AVCC and AVSS as VREF
    // A0 selected as analog channel
    //******************************

    ADCMCTL0 = 0;


    //************************************
    // After selecting XT1 functions for
    // port lines, clear the fault flag
    //************************************

    do
   {
       CSCTL7 &= ~(XT1OFFG | DCOFFG);      // clear XT1 and DCO fault flags
       SFRIFG1 &= ~OFIFG;                  // clear osc fault interrupt flag
   }while (SFRIFG1 & OFIFG);               // test osc fault flag



    //*****************************************************************
    // We will not turn the ADC on yet, since it consumes about
    // 280uA when on. We will turn it on just before we need it.
    //*****************************************************************


    //*********************************
    // Initialize TIMER0
    //
    // TIMER0 is used for low speed
    // timing events, such as 10mS
    // wake-up.
    //
    // Clock source ACLK (39062.5 HZ)
    // ID Divider = /1
    // IDEX Divider = /1
    // Continuous mode
    // 16 bit
    //*********************************

    //*****************************************
    // Setup compare register for TIMER0, CCR0
    // for first compare in 10mS from time
    // Timer0 is enabled. Timer is not setup
    // or started yet.
    //*****************************************

    TB0CCR0 = TIMB0_WAKEUP_CCR0;


    //************************************************************
    // TB0CTL0, TIMER0, Compare 0 Control
    //
    // Bits 15:14, CM = 00, No Capture
    // Bits 13:12, CCIS = 00, CCI0A
    // Bit 11, SCS = 0, Async Capture
    // Bits 10:9, CLLD = 00, TB0CL0 loads on write
    // Bit 8,, CAP = 0, Compare mode
    // Bits 7:6:5, OUTMODE = 000, OUT bit value
    // Bit 4, CCIE = 1, Compare 0 interrupt enabled
    // Bit 3 CCI, Read Only, Input signal
    // Bit 2, OUT = 0, Output low
    // Bit 1, COV, Flag, 1=Capture Overflow occurred
    // Bit 0, CCIFG, Flag, 1=Interrupt pending
    //*************************************************************

    TB0CCTL0 = \
                CAP_0 | \
                CCIS_0 | \
                SCS__ASYNC | \
                CLLD_0 | \
                CAP_0 | \
                OUTMOD_0 | \
                CCIE_1 | \
                OUT_0;

    //***********************************************************
    // TB0EX0, Timer0 Expansion Register
    //
    // Bits 15-3, Reserved
    // Bits 2:1:0 = 000, Divide source clock input by 1
    //***********************************************************

    TB0EX0 = TBIDEX_0;          // divide by 1


    //***********************************************************
    // TB0CTL, TIMER0 Control
    //
    // Bit 15, Reserved
    // Bits 14:13, TBCLGRP = 00, Each TBxCLn latch is independent
    // Bits 12:11, CNTL = 00, 16 bit mode
    // Bit 10, Reserved
    // Bits 9:8, TBSSEL = 01, ACLK Source
    // Bits 7:6, ID = 00, Divide by 1
    // Bits 5:4, MC = 10, Continuous mode
    // Bit 3, Reserved
    // Bit 2, TBCLR = 0, Set this bit to clear timer
    // Bit 1, TBIE = 0, Interrupts disabled (THIS IS TIMER OVERFLOW)
    // Bit 0, TBIFG, Interrupt flag
    //
    // TIMER STARTS NOW
    //
    //************************************************************

    TB0CTL = \
            TBCLGRP_0 | \
            CNTL_0 | \
            TBSSEL__ACLK | \
            ID_0 | \
            MC__CONTINUOUS | \
            TBIE_0;


    //*********************************
    // Initialize TIMER1
    //
    // TIMER1 is used for high speed
    // timing events such as 50uS
    // core set and reset.
    //
    // Clock source SMCLK (10MHZ)
    // ID Divider = /1
    // Continuous mode
    // 16 bit
    //*********************************


    //*****************************************
    // Setup compare register for TIMER1, CCR0
    // for first compare in 50uS from time
    // Timer1 is enabled. Timer is not setup
    // or started yet.
    //*****************************************

    TB1CCR0 = TIMB1_CORE_SET_CCR0;


    //************************************************************
    // TB1CCTL0, TIMER1, Compare 0 Control
    //
    // Bits 15:14, CM = 00, No Capture
    // Bits 13:12, CCIS = 00, CCI0A
    // Bit 11, SCS = 0, Async Capture
    // Bits 10:9, CLLD = 00, TB0CL0 loads on write
    // Bit 8,, CAP = 0, Compare mode
    // Bits 7:6:5, OUTMODE = 000, OUT bit value
    // Bit 4, CCIE = 1, Compare 0 interrupt enabled
    // Bit 3 CCI, Read Only, Input signal
    // Bit 2, OUT = 0, Output low
    // Bit 1, COV, Flag, 1=Capture Overflow occurred
    // Bit 0, CCIFG, Flag, 1=Interrupt pending
    //*************************************************************

    TB1CCTL0 = \
                CAP_0 | \
                CCIS_0 | \
                SCS__ASYNC | \
                CLLD_0 | \
                CAP_0 | \
                OUTMOD_0 | \
                CCIE_0 | \
                OUT_0;

    //***********************************************************
    // TB1EX0, Timer1 Expansion Register
    //
    // Bits 15-3, Reserved
    // Bits 2:1:0 = 000, Divide source clock input by 1
    //***********************************************************

    TB1EX0 = TBIDEX_0;          // divide by 1 ////



    //***********************************************************
    // TB1CTL, TIMER1 Control
    //
    // Bit 15, Reserved
    // Bits 14:13, TBCLGRP = 00, Each TBxCLn latch is independent
    // Bits 12:11, CNTL = 00, 16 bit mode
    // Bit 10, Reserved
    // Bits 9:8, TBSSEL = 10, SMCLK Source
    // Bits 7:6, ID = 11, Divide by 8 (10MHZ/8 = 1.25MHZ)
    // Bits 5:4, MC = 10, TIMER1 continuous mode
    // Bit 3, Reserved
    // Bit 2, TBCLR = 0, Set this bit to clear timer
    // Bit 1, TBIE = 0, Interrupts disabled for now
    // Bit 0, TBIFG, Interrupt flag
    //
    //
    //************************************************************

    TB1CTL = \
            TBCLGRP_0 | \
            CNTL_0 | \
            TBSSEL__SMCLK | \
            ID__8 | \
            MC__CONTINUOUS | \
            TBIE_0;

    //**********************************************************************
    // Configure SAC1
    //
    // SAC1OA, SAC OA Control Register
    //
    // Bits 15-11, Reserved
    // Bit 10, SACEN = 1, SAC all modules enabled
    // Bit 9, OAPM = 1, Low speed and power
    // Bit 8, OAEN = 1, SAC OA is enabled, normal mode
    // Bit 7, NMUXEN = 1, all negative sources connected to OA negative port
    // Bit 6, Reserved
    // Bits 5:4, NSEL = 01, PGA source selected
    // Bit 3, PMUXEN = 1, all positive sources connected to OA positive port
    // Bit 2, Reserved
    // Bit 1:0, PSEL = 01, 12 bit DAC as input to OA
    //***********************************************************************

    SAC1OA = \
                SACEN | \
                OAPM | \
                OAEN | \
                NMUXEN | \
                NSEL_1 | \
                PMUXEN | \
                PSEL_1;

    //***********************************************************************
    // SAC1PGA, SAC1 PGA Control Register
    //
    // Bits 15:7, Reserved
    // Bits 6:5:4, GAIN = 000, Gain = 1
    // Bits 3:2, Reserved
    // Bits 1:0, MSEL = 01, Follower mode
    //************************************************************************

    SAC1PGA = \
                MSEL0;


    //***********************************************************************
    // SAC1DAC, SAC DAC Control Register
    //
    // Bits 15:13, Reserved
    // Bits 12, DACSREF = 0, Primary reference selected (DVCC for this part)   *** TEST ***
    // Bits 11:10, Reserved
    // Bits 9:8, DACLSEL = 00, DAC latch loads when DACDAT written
    // Bits 7:3, Reserved
    // Bit 2, DACDMAE = 0, DMA request disabled
    // Bit 1, DACIE = 0, Interrupts disabled
    // Bit 0, DACEN = 1, SAC DAC enabled
    //***********************************************************************

    SAC1DAC = \
            DACSREF_0 | \
            DACLSEL_0 | \
            DACDMAE_0 | \
            DACIE_0 | \
            DACEN_1;

    //************************************************************************
    // Initialize MPY32 module
    // Module will be setup for 16x16 unsigned integer multiplication.
    //
    // MPY32CTL0
    //
    // Bits 15-10, Reserved
    // Bit 9, MPYDLY32 = 1, Writes are delayed until 32bit result ready
    // Bit 8, MPYDLYWRTEN = 1, Writes are delayed
    // Bit 7, MPYOP2_32 = 0, Operand2 is 16 bits
    // Bit 6, MPYOP1_32 = 0, Operand3 is 16 bits
    // Bits 5:4, MPYMx = 00, MPY-Multiply
    // Bit 3, MPYSAT = 0, Saturation mode disabled
    // Bit 2, MPYFRAC = 0, Fractional mode disabled
    // Bit 1, Reserved
    // Bit 0, MPYC = 0, No carry for result
    //*************************************************************************

    MPY32CTL0 = \
                MPYDLY32_1 | \
                MPYDLYWRTEN_1 | \
                MPYOP2_32_0 | \
                MPYOP1_32_0 | \
                MPYM_0 | \
                MPYSAT_0 | \
                MPYFRAC__DISABLE | \
                MPYC_0;


    //***************************************
    // Initialization complete
    // Enable global interrupts
    //***************************************

//    _enable_interrupts();


}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    似乎您正在 使 LPM3中的 HFXT 保持活动(10MHz),以保持 ACLK 的运行。

    我在 FR2355数据表中没有看到 HFXT 的功率规格,但(例如)。FR5969数据表(SLAS704F)表5-5显示其 HFXT 在8MHz 时大约需要120uA。

    从 REFO 运行 ACLK 可能会更好,该操作只需要大约20uA。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢布鲁斯。

     我将尝试运行 ACLK 关闭 REFO,并查看发生了什么。 我有点担心可再生能源对温度的耐受性,但经过进一步考虑,这可能不是一个如此糟糕的交易。 我会让每个人都知道结果。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,格雷戈里,

    是否有基于 Bruce 建议的更新?  您仍有问题吗?  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的,问题已解决。 我将 MCLK 和 SMCLK 的时钟源更改为将 REFO 与 FLL 一起使用(设置为8MHZ)。 ACLK 使用 REFO。 HFXT 已关闭。 电流从325uA 降至68uA。 68uA 数字低于预期,但我对此感到高兴。