This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR5994:使用ADC12MEM0以外的内存插槽进行ADC存储

Guru**** 2387880 points
Other Parts Discussed in Thread: MSP-EXP430FR5994
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1089910/msp430fr5994-using-a-memory-slot-other-than-adc12mem0-for-adc-storage

部件号:MSP430FR5994
主题中讨论的其他部件:MSP-EXP430FR5994

大家好,我正在 使用MSP-EXP430FR5994开发板上基本ADC的MSP430Ware示例代码。 在代码上,它使用MEM0和支持基础设施(如标志0)进行转换。 下面是我的修改;我使用了MEM2和标志2进行转换。

#include <msp430.h>
#include <stdio.h>

int main(void)
{
    WDTCTL = WDTPW | WDTHOLD;               // Stop WDT

    // GPIO Setup
    P1OUT &= ~BIT0;                         // Clear LED to start
    P1DIR |= BIT0;                          // Set P1.0/LED to output
    P1SEL1 |= BIT2;                         // Configure P1.2 for ADC input (See p369, p88 of specific for pin config details.)
    P1SEL0 |= BIT2;                         // There are two Pin Select bits (p88 of specifics, we are given that P1.2 corresponds to A2.)

    // Disable the GPIO power-on default high-impedance mode to activate
    // previously configured port settings (p92)
    PM5CTL0 &= ~LOCKLPM5;

    // Configure ADC12
    ADC12CTL0 = ADC12SHT0_2 | ADC12ON;      // Sampling time, S&H=16, ADC12 on [p893, CTL0 = control 0, SHT0_2 = sample & hold time, knowledge of register value from p88_s]
    ADC12CTL1 = ADC12SHP;                   // Use sampling timer [p895, Sampler uses sampling timer (not sure what that is yet)]
    ADC12CTL2 |= ADC12RES_2;                // 12-bit conversion results [p897, RES means resolution, _2 means 12 bits]
    ADC12MCTL2 |= ADC12INCH_2;
    ADC12IER0 |= ADC12IE0 | ADC12IE2;                  // Enable ADC conv complete interrupt [p903, means "interrupt enable register 0". Enables or disables the interrupt request for ADC12IFG0 bit (what the ?)]
    printf("Got here.\n");

    while (1)
    {
        //printf("Got there.\n");
        __delay_cycles(5000);
        ADC12CTL0 |= ADC12ENC | ADC12SC;    // Start sampling/conversion [p893, ENC = enable conversion, SC = start conversion. difference between the two = idfk, but remember to have both set]
        //int memval = ADC12MEM2;
        //printf("%d\n", memval);

        __bis_SR_register(LPM0_bits | GIE); // LPM0, ADC12_ISR will force exit

       // printf("Got nowhere.\n");
        __no_operation();                   // For debugger
    }
}

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = ADC12_B_VECTOR
__interrupt void ADC12_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC12_B_VECTOR))) ADC12_ISR (void)
#else
#error Compiler not supported!
#endif
{
    switch(__even_in_range(ADC12IV, ADC12IV__ADC12RDYIFG))
    {
        case ADC12IV__NONE:        break;   // Vector  0:  No interrupt
        case ADC12IV__ADC12OVIFG:  break;   // Vector  2:  ADC12MEMx Overflow
        case ADC12IV__ADC12TOVIFG: break;   // Vector  4:  Conversion time overflow
        case ADC12IV__ADC12HIIFG:  break;   // Vector  6:  ADC12BHI
        case ADC12IV__ADC12LOIFG:  break;   // Vector  8:  ADC12BLO
        case ADC12IV__ADC12INIFG:  break;   // Vector 10:  ADC12BIN
        case ADC12IV__ADC12IFG0:            // Vector 12:  ADC12MEM0 Interrupt
            if (ADC12MEM0 >= 0x7ff){           // ADC12MEM0 = A1 > 0.5AVcc?
                P1OUT |= BIT0;              // P1.0 = 1
            }
            else{
                P1OUT &= ~BIT0;             // P1.0 = 0
            }
            int memval = ADC12MEM0;             // Memory stored in MEM0, because it was set from above.
            printf("%d\n", memval);
                // Exit from LPM0 and continue executing main
                __bic_SR_register_on_exit(LPM0_bits);
            break;
        case ADC12IV__ADC12IFG1:   break;   // Vector 14:  ADC12MEM1
        case ADC12IV__ADC12IFG2:   break;   // Vector 16:  ADC12MEM2
            if (ADC12MEM2 >= 0x7ff){           // ADC12MEM0 = A1 > 0.5AVcc?
                P1OUT |= BIT0;              // P1.0 = 1
            }
            else{
                P1OUT &= ~BIT0;             // P1.0 = 0
            }
            int memval = ADC12MEM2;             // Memory stored in MEM0, because it was set from above.
            printf("%d\n", memval);
                // Exit from LPM0 and continue executing main
                __bic_SR_register_on_exit(LPM0_bits);
            break;
        case ADC12IV__ADC12IFG3:   break;   // Vector 18:  ADC12MEM3
        case ADC12IV__ADC12IFG4:   break;   // Vector 20:  ADC12MEM4
        case ADC12IV__ADC12IFG5:   break;   // Vector 22:  ADC12MEM5
        case ADC12IV__ADC12IFG6:   break;   // Vector 24:  ADC12MEM6
        case ADC12IV__ADC12IFG7:   break;   // Vector 26:  ADC12MEM7
        case ADC12IV__ADC12IFG8:   break;   // Vector 28:  ADC12MEM8
        case ADC12IV__ADC12IFG9:   break;   // Vector 30:  ADC12MEM9
        case ADC12IV__ADC12IFG10:  break;   // Vector 32:  ADC12MEM10
        case ADC12IV__ADC12IFG11:  break;   // Vector 34:  ADC12MEM11
        case ADC12IV__ADC12IFG12:  break;   // Vector 36:  ADC12MEM12
        case ADC12IV__ADC12IFG13:  break;   // Vector 38:  ADC12MEM13
        case ADC12IV__ADC12IFG14:  break;   // Vector 40:  ADC12MEM14
        case ADC12IV__ADC12IFG15:  break;   // Vector 42:  ADC12MEM15
        case ADC12IV__ADC12IFG16:  break;   // Vector 44:  ADC12MEM16
        case ADC12IV__ADC12IFG17:  break;   // Vector 46:  ADC12MEM17
        case ADC12IV__ADC12IFG18:  break;   // Vector 48:  ADC12MEM18
        case ADC12IV__ADC12IFG19:  break;   // Vector 50:  ADC12MEM19
        case ADC12IV__ADC12IFG20:  break;   // Vector 52:  ADC12MEM20
        case ADC12IV__ADC12IFG21:  break;   // Vector 54:  ADC12MEM21
        case ADC12IV__ADC12IFG22:  break;   // Vector 56:  ADC12MEM22
        case ADC12IV__ADC12IFG23:  break;   // Vector 58:  ADC12MEM23
        case ADC12IV__ADC12IFG24:  break;   // Vector 60:  ADC12MEM24
        case ADC12IV__ADC12IFG25:  break;   // Vector 62:  ADC12MEM25
        case ADC12IV__ADC12IFG26:  break;   // Vector 64:  ADC12MEM26
        case ADC12IV__ADC12IFG27:  break;   // Vector 66:  ADC12MEM27
        case ADC12IV__ADC12IFG28:  break;   // Vector 68:  ADC12MEM28
        case ADC12IV__ADC12IFG29:  break;   // Vector 70:  ADC12MEM29
        case ADC12IV__ADC12IFG30:  break;   // Vector 72:  ADC12MEM30
        case ADC12IV__ADC12IFG31:  break;   // Vector 74:  ADC12MEM31
        case ADC12IV__ADC12RDYIFG: break;   // Vector 76:  ADC12RDY
        default: break;
    }
}

由于我以外的原因,我无法让MEM2工作;当Vcc高于Vcc/2时,指示灯未激活。 如果需要更多信息来解决此问题,请告诉我。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    要从MEM2/MCTL2开始,您需要设置CSTARTADD=2 [Ref UG (SLU367P) Table 34-7],类似于:

    >ADC12CTL3 |= ADC12CSTARTADD_2;//使用MEM2/MCTL2

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    通读文档,它表示它是“ADC起始地址”,并且“转换存储器寄存器用于单个转换或序列中的第一个转换”。 这是否意味着如果我为两个ADC样本的序列将其设置为MEM2,则第二个总是转到MEM3?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的