This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR5994:ADC采样速率与预期相差很大

Guru**** 2540440 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1090650/msp430fr5994-adc-sampling-at-a-much-different-rate-than-expected

部件号:MSP430FR5994

大家好,我有一些代码使用32Hz PWM计时器作为ADC采样的基础,在两个单独的通道上,存储在两个单独的存储器中。 当然,我预计ADC的采样频率为32Hz。 但是,我的采样速度似乎要慢得多,大约为4Hz,而且两个ADC信道之间存在明显的延迟。 我通过在同一信号上同时运行两个ADC信道来测试此情况,并估计0.2 秒的延迟。

下面是我的代码,如果它有帮助的话。 我一直依靠printf函数通过USB电缆进行调试。 为了获得两个ADC通道的比较结果,我使用了第116行,其中我用ADC12MEM3来减去ADC12MEM4。

#include <msp430.h>
#include <stdio.h>

int memval3_old = 0;    //Old is for storing old ADC values
int memval4_old = 0;
int memval3_new = 0;    //New is for storing new ADC values. By what metric is this considered necessary documentation?
int memval4_new = 0;
double voltage_difference_new, voltage_difference_old, voltage_difference_range, voltage_difference_doppler;

int main(void)
{
    WDTCTL = WDTPW | WDTHOLD;               // Stop WDT

    // GPIO Setup
    P1OUT &= ~BIT0;                         // Clear LED to start
    P1DIR |= BIT0 | BIT1 | BIT2;
    P1SEL1 |= BIT3 | BIT4 ;
    P1SEL0 |= BIT2 | BIT3 | BIT4 ;                 // Check p88-90_s for what the hell we're doing in the last 3 lines
                                            // 1.2 set to TA1.1, 1.3 and 1.4 set to ADC input (A3)

    PJSEL0 = BIT4 | BIT5;                   // For XT1? (p118_s)

    // Disable the GPIO power-on default high-impedance mode to activate
    // previously configured port settings
    PM5CTL0 &= ~LOCKLPM5;
    P1OUT |= BIT0;

    // Clock System Setup
    CSCTL0_H = CSKEY_H;                     // Unlock CS registers
    CSCTL1 = DCOFSEL_3;                     // Set DCO to 4MHz (p105)
    CSCTL2 = SELA__VLOCLK | SELS__DCOCLK | SELM__DCOCLK;   // Set clock source
    CSCTL3 = DIVA__1 | DIVS__4 | DIVM__1;   // Set all dividers, clock speed 1MHz
    CSCTL4 &= ~LFXTOFF;                     // Something related to the 32kHz oscillator, idfk

    do
    {
        CSCTL5 &= ~LFXTOFFG;                // Clear XT1 fault flag
        SFRIFG1 &= ~OFIFG;
    } while (SFRIFG1 & OFIFG);              // Test oscillator fault flag

    ADC12CTL0 = ADC12SHT0_0 | ADC12ON;      // Sampling time, S&H=4, ADC12 on [p893, CTL0 = control 0, SHT0_0 = sample & hold time, knowledge of register value from p88_s]

    ADC12CTL1 = ADC12SHP | ADC12SHS_4 | ADC12CONSEQ_3; // Use TA1.1 to trigger, (SHP means using sample timer (p897), SHS means "sample-and-hold source select" (p895, p84_s)
                                                       // which selects which source is used to activate sampling (4 being TA1.1 because of p84_s), CONSEQ_3 = Conversion sequence select,
                                                       // 3 means repeated-multiple-channel which means multiple channels are converted and sampled, memory gets overriden everytime (p881)
    ADC12CTL2 |= ADC12RES_2;                // 12-bit conversion results, p897
    ADC12CTL3 |= ADC12CSTARTADD_3;          // Use MEM3/MCTL3 as first, p898

    ADC12MCTL3 = ADC12INCH_3;               // A3 ADC input select from INCH (p901), output to MEM3
    ADC12MCTL4 = ADC12INCH_4 | ADC12EOS;    // A4 ADC input select, output to MEM4, also setting EOS bit at A4

    ADC12IER0 |= ADC12IE3 | ADC12IE4 ;      // Enable ADC interrupt [IER = interrupt enable, for IFG0 bit, which tells us when the sequence is complete]
    ADC12CTL0 |= ADC12ENC | ADC12SC;        // Start sampling/conversion

    // Configure TimerA1.1 to periodically trigger the ADC12 (Change later)
    TA1CCR0 = 31250-1;                       // PWM Period for TA1, change to 32Hz, 31250/1000000 = /32
    TA1CCTL1 = OUTMOD_3;                    // TACCR1 set/reset (Shape of set/reset in p652)

    TA1CCR1 = 15625;                         // TACCR1 PWM Duty Cycle
    TA1CTL = TASSEL__SMCLK | MC__UP;        // ACLK, up mode
    printf("122\n");
    __bis_SR_register(LPM0_bits | GIE);     // Enter LPM0, enable interrupts

    //int memval = ADC12MEM0;             // Memory stored in MEM0, because it was set from above.
    //printf("%d\n", memval);
}

// ADC12 interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=ADC12_B_VECTOR
__interrupt void ADC12ISR (void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC12_B_VECTOR))) ADC12ISR (void)
#else
#error Compiler not supported!
#endif
{
    switch(__even_in_range(ADC12IV, ADC12IV__ADC12RDYIFG))
    {
        //Some flag conditions, more important than we might originally think
        case ADC12IV__NONE:        break;   // Vector  0:  No interrupt
        case ADC12IV__ADC12OVIFG:  break;   // Vector  2:  ADC12MEMx Overflow
        case ADC12IV__ADC12TOVIFG: break;   // Vector  4:  Conversion time overflow
        case ADC12IV__ADC12HIIFG:  break;   // Vector  6:  ADC12BHI
        case ADC12IV__ADC12LOIFG:  break;   // Vector  8:  ADC12BLO
        case ADC12IV__ADC12INIFG:  break;   // Vector 10:  ADC12BIN
        case ADC12IV__ADC12IFG0:            // Vector 12:  ADC12MEM0 Interrupt
            break;
        case ADC12IV__ADC12IFG1:   break;   // Vector 14:  ADC12MEM1
        case ADC12IV__ADC12IFG2:   break;   // Vector 16:  ADC12MEM2
        case ADC12IV__ADC12IFG3:            // Vector 18:  ADC12MEM3
            /*if (ADC12MEM3 >= 0x7ff){         // ADC12MEM3 = A1 > 0.5AVcc?
                P1OUT |= BIT0;              // P1.0 = 1
            }
            else
                P1OUT &= ~BIT0;{             // P1.0 = 0
            }*/
            //memval3_old = memval3_new;      //Move old memory into new
            //memval3_new = ADC12MEM3;             // Memory stored in MEM3
            //printf("The value of old MEM3 is %d\n", memval3_old);
            //printf("The value of new MEM3 is %d\n", memval3_new);
            break;
        case ADC12IV__ADC12IFG4:           // Vector 20:  ADC12MEM4
            /*if (ADC12MEM4 >= 0x7ff){         // ADC12MEM4 = A1 > 0.5AVcc?
                P1OUT |= BIT1;              // P1.0 = 1
            }
            else
                P1OUT &= ~BIT1;{             // P1.0 = 0
            }*/
            //memval4_old = memval4_new;
            //memval4_new = ADC12MEM4;             // Memory stored in MEM4

            //printf("The value of old MEM4 is %d\n", memval4_old);
            //printf("The value of new MEM3 is %d\n", memval3_new);
            //printf("The value of new MEM4 is %d\n", memval4_new);
            printf("%d\n", ADC12MEM3 - ADC12MEM4);

            //voltage_difference_new = fabs((memval3_new - memval4_new)*3.3/4096); // These values are both +ve, rising edge
            //voltage_difference_old = fabs((memval3_old - memval4_old)*3.3/4096); // These values are both +ve, falling edge

            //voltage_difference_range = ((voltage_difference_new + voltage_difference_old)/2);
            //voltage_difference_doppler = ((voltage_difference_new - voltage_difference_old)/2);

            //printf("%3f\n", voltage_difference_new);
            //printf("%3f\n", voltage_difference_old);

            //printf("%3f\n", voltage_difference_range);
            //printf("%3f\n", voltage_difference_doppler);
            break;
        case ADC12IV__ADC12IFG5:   break;   // Vector 22:  ADC12MEM5
        case ADC12IV__ADC12IFG6:   break;   // Vector 24:  ADC12MEM6
        case ADC12IV__ADC12IFG7:   break;   // Vector 26:  ADC12MEM7
        case ADC12IV__ADC12IFG8:   break;   // Vector 28:  ADC12MEM8
        case ADC12IV__ADC12IFG9:   break;   // Vector 30:  ADC12MEM9
        case ADC12IV__ADC12IFG10:  break;   // Vector 32:  ADC12MEM10
        case ADC12IV__ADC12IFG11:  break;   // Vector 34:  ADC12MEM11
        case ADC12IV__ADC12IFG12:  break;   // Vector 36:  ADC12MEM12
        case ADC12IV__ADC12IFG13:  break;   // Vector 38:  ADC12MEM13
        case ADC12IV__ADC12IFG14:  break;   // Vector 40:  ADC12MEM14
        case ADC12IV__ADC12IFG15:  break;   // Vector 42:  ADC12MEM15
        case ADC12IV__ADC12IFG16:  break;   // Vector 44:  ADC12MEM16
        case ADC12IV__ADC12IFG17:  break;   // Vector 46:  ADC12MEM17
        case ADC12IV__ADC12IFG18:  break;   // Vector 48:  ADC12MEM18
        case ADC12IV__ADC12IFG19:  break;   // Vector 50:  ADC12MEM19
        case ADC12IV__ADC12IFG20:  break;   // Vector 52:  ADC12MEM20
        case ADC12IV__ADC12IFG21:  break;   // Vector 54:  ADC12MEM21
        case ADC12IV__ADC12IFG22:  break;   // Vector 56:  ADC12MEM22
        case ADC12IV__ADC12IFG23:  break;   // Vector 58:  ADC12MEM23
        case ADC12IV__ADC12IFG24:  break;   // Vector 60:  ADC12MEM24
        case ADC12IV__ADC12IFG25:  break;   // Vector 62:  ADC12MEM25
        case ADC12IV__ADC12IFG26:  break;   // Vector 64:  ADC12MEM26
        case ADC12IV__ADC12IFG27:  break;   // Vector 66:  ADC12MEM27
        case ADC12IV__ADC12IFG28:  break;   // Vector 68:  ADC12MEM28
        case ADC12IV__ADC12IFG29:  break;   // Vector 70:  ADC12MEM29
        case ADC12IV__ADC12IFG30:  break;   // Vector 72:  ADC12MEM30
        case ADC12IV__ADC12IFG31:  break;   // Vector 74:  ADC12MEM31
        case ADC12IV__ADC12RDYIFG: break;   // Vector 76:  ADC12RDY
        default: break;
    }
}

这是一个我想要的时间顺序的例子。

请告诉我代码的哪一部分不正确,因为这是基于 16Hz ADC采样器代码

编辑:问题已更改,请参阅回复4以了解有关当前问题的更多信息。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Oscar:

    是否可以尝试从代码中删除printf语句? printf是一个复杂的函数,不应从计时关键代码调用。 相反,我建议切换ISR中的LED,以确认采样率正确。 如果您可以使用示波器或逻辑分析仪,这将是确认采样率的好方法。

    此致,

    Evan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Evan:

    我确实相信打印机是造成这种情况的好机会,但我想知道如何在不使用打印机的情况下显示结果。 虽然您的回答正确,但我应该能够使用LED指示灯运行进一步的测试。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Oscar:

    您能否确认在没有printf ISR的情况下,代码的计时工作正常? 一旦我们有了工作基线,我们就可以找到"打印"数据的最佳方式。

    谢谢!

    Evan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Evan:

    我发现我的代码计时也不能正常工作。 现在,MEM3在MEM4结束时就开始收集数据,这使我获得了66kHz的采样率,我通过ADC标记切换输出引脚发现了这种采样率。 我猜这与ADC12EOS位没有正确结束序列有关。

    谢谢!

    奥斯卡