你(们)好 我正在尝试使用 MSP430FR5994通过UART传输从1到100的序列。 我无法这样做,因为我的代码似乎不接受变量值。
我的代码:
#include <msp430.h>
char RXbuffer[32];
const unsigned char maxRXbytes = sizeof(RXbuffer);
unsigned char RXbytes = 0;
int i = 0;
char message[] = i;
const unsigned char messageLength = sizeof(message);
unsigned char TXbytes = 0;
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop Watchdog
// Configure GPIO
P2SEL0 &= ~(BIT0 | BIT1);
P2SEL1 |= (BIT0 | BIT1); // USCI_A0 UART operation (p93_s)
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Startup clock system with max DCO setting ~8MHz
CSCTL0_H = CSKEY_H; // Unlock CS registers
CSCTL1 = DCOFSEL_3 | DCORSEL; // Set DCO to 8MHz
CSCTL2 = SELA__VLOCLK | SELS__DCOCLK | SELM__DCOCLK;
CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers
CSCTL0_H = 0; // Lock CS registers
// Configure USCI_A0 for UART mode
UCA0CTLW0 = UCSWRST; // Put eUSCI in reset (p788)
UCA0CTLW0 |= UCSSEL__SMCLK; // CLK = SMCLK
// Baud Rate calculation for 19200
// 8000000/(16*19200) = 26.042
// Fractional portion = 0.042
// User's Guide Table 21-4: UCBRSx = 0xD6
// UCBRFx = int ( (52.083-52)*16) = 1
UCA0BRW = 26; // 8000000/16/19200, p789
UCA0MCTLW |= UCOS16 | UCBRF_1 | 0xD600; // UCOS16 = Oversampling enable, used when high frequency clk is used, probably divides everything by 16, UCBRF = fine turner when UCOS16 is active
// 0xD600 is for first 8 bits,
UCA0CTLW0 &= ~UCSWRST; // Initialize eUSCI
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
while(1){
__delay_cycles(20000);
UCA0IE |= UCTXIE;
i++;
__bis_SR_register(LPM3_bits | GIE); // Enter LPM3, interrupts enabled
__no_operation(); // For debugger
}
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=EUSCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(EUSCI_A0_VECTOR))) USCI_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(UCA0IV,USCI_UART_UCTXCPTIFG))
{
case USCI_NONE: break;
case USCI_UART_UCRXIFG:
break;
case USCI_UART_UCTXIFG: //TXIFG = transmission flag, needs manual activation
// Transmit the byte
//UCA0TXBUF = UCA0RXBUF;
UCA0TXBUF = message[TXbytes++]; //TXBUF = Transmit Buffer, p791
// If last byte sent, disable the interrupt
if(TXbytes == messageLength)
{
UCA0IE &= ~UCTXIE;
TXbytes = 0;
}
__bic_SR_register_on_exit(LPM3_bits);
break;
case USCI_UART_UCSTTIFG: break;
case USCI_UART_UCTXCPTIFG: break;
default: break;
}
}
如果需要更多信息来解决此问题,请告诉我;我对此非常陌生。