This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430F6433:使用2 mm 聚碳酸酯实现RO系统电容式触摸感应是否可行?

Guru**** 2778945 points

Other Parts Discussed in Thread: MSP430FR6889, MSP430F6433

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/633051/msp430f6433-is-it-possible-to-realize-capacitive-touch-sensing-of-ro-system-with-2-mm-polycarbonate

部件号:MSP430F6433
主题中讨论的其他部件:MSP430FR6889,MSP-EXP430F5529

你好。

我有疑问。

我希望通过MSP430F6433或MSP430FR6889实现RO系统的电容式触摸感应。

使用2 mm 聚碳酸酯可以实现RO系统的电容式触摸感应吗?

对于MSP-EXP430F5529的触摸传感器演示,假定灵敏度为。

此致,

Uchida-k