This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430F5659:MCLK = 20MHz,USB和BSL的UCS设置

Guru**** 2589280 points
Other Parts Discussed in Thread: MSP430F5659

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/629730/msp430f5659-ucs-settings-for-mclk-20mhz-usb-and-bsl

部件号:MSP430F5659

您好,

我需要为MSP430F5659器件设置时钟以获得最佳性能。  根据先前与USB I相关的帖子,MSP430F5659被限制为20 MHz。

由于XT2是24 MHz晶体,由于FLL分频器设置(0.8333 的非整数值),我们无法实现20 MHz MCLK

由于XT2是4 MHz晶体,我们无法实现20MHz,因为20/4=5,DIV选项为1,2,4,8,12,16。

由于XT2不是4,8,12或24 MHz,我们无法使用MSP430 BSL中的自动XT2检测。

我的问题是,XT2的哪个值允许我拥有20 MHz MCLK,48 MHz USB PLL并使用MSP430 BSL自动XT2检测?

有什么建议?

谢谢

太棒了!