This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP-GANG430:组编程器问题

Guru**** 2608385 points
Other Parts Discussed in Thread: MSP430F425, MSP-GANG

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/655137/msp-gang430-gang-programmer-issue

部件号:MSP-GANG430

我一直在使用MSP430F425和427 Seven系列的MSP-Gang编程器,但突然,它今天就停止工作了。 弹出错误23,自检时出现了许多错误。 请告诉我接下来应该做什么,因为这是我们唯一的程序员。 自检结果如下:  

=== MSP-GANG自检结果(2018年1月10日星期三12:20:57)===

适配器序列号------- :1510.0533万
硬件------- :G430:01.04
访问键-------- :MSP-Gang程序员
芯片编号--:8426 1147 2400 1100
API固件---:MSP-Gang A430: 01.02 .05.00
启动固件---:G430BOOT B430: 01.00 .02.00
GUI软件---:MSP-Gang-GUI G430: 01.02 .05.00
DLL软件--------:MSP-Gang-DLL D430: 01.02 .05.00

=================== 测试结果===========


否。名称参数限制结果状态


1:数据总线(全部为低) 0x0000 (0x0000 - 0x0000)结果:0x00 ... >>确定<<
2:数据总线(全部高) 0x00FF (0xFFFF - 0xFFFF)结果:0xFFFF ... >>确定<<
3:数据总线(D-0 HI ) 0x0001 (0x0101-0x0101)结果0101结果:0x0101... >>确定<<
4:数据总线(D-1 HI ) 0x0002 (0x0202-0x0202)结果0202结果:0x0202... >>确定<<
5:数据总线(D-2 HI ) 0x0004 (0x0404-0x0404)结果0404结果:0x0404... >>确定<<
6:数据总线(D-3 HI ) 0x0008 (0x0808-0x0808)结果0808结果:0x0808... >>确定<<
7:数据总线(D-4 HI) 0x0010 (0x1010 - 0x1010)结果:0x1010 ... >>确定<<
8:数据总线(D-5 HI ) 0x0020 (0x2020-0x2020)结果2020结果:0x2020... >>确定<<
9:数据总线(D-6 HI ) 0x0040 (0x4040-0x4040)结果4040结果:0x4040... >>确定<<
10:数据总线(D-7 HI ) 0x0080 (0x8080 - 0x8080)结果:0x8080... >>确定<<

11:Data-2总线(全部为低) 0x0000 (0x0000 - 0x0000)结果:0x00... >>确定<<
12:数据2总线(全部高) 0x00FF (0xFFFF - 0xFFFF)结果:0xFFFF ... >>确定<<
13:Data-2总线(D2-0 HI ) 0x0001 (0x0101 - 0x0101)结果:0x0101... >>确定<<
14:数据2总线(D2-1 HI ) 0x0002 (0x0202-0x0202)结果0202结果:0x0202... >>确定<<
15:数据2总线(D2-2 HI ) 0x0004 (0x0404 - 0x0404)结果:0x0404... >>确定<<
16:数据2总线(D2-3 HI ) 0x0008 (0x0808 - 0x0808)结果:0x0808... >>确定<<
17:数据2总线(D2-4 HI ) 0x0010 (0x1010 - 0x1010)结果:0x1010... >>确定<<
18:数据2总线(D2-5 HI ) 0x0020 (0x2020 - 0x2020)结果:0x2020... >>确定<<
19:Data-2总线(D2-6 HI ) 0x0040 (0x4040-0x4040)结果4040结果:0x4040... >>确定<<
20:Data-2总线(D2-7 HI ) 0x0080 (0x8080 - 0x8080)结果:0x8080... >>确定<<

21:VCC Target-1 (全部关闭) 0.00 V (0.00 至0.30)结果:0.02 V... >>确定<<
22:VCC Target-2 (全部关闭) 0.00 V (0.00 至0.30)结果:0.01 V... >>确定<<
23:VCC Target-3 (全部关闭) 0.00 V (0.00 至0.30)结果:0.01 V... >>确定<<
24:VCC Target-4 (全部关闭) 0.00 V (0.00 至0.30)结果:0.01 V... >>确定<<
25:VCC Target-5 (全部关闭) 0.00 V (0.00 至0.30)结果:0.01 V... >>确定<<
26:VCC Target-6 (全部关闭) 0.00 V (0.00 至0.30)结果:0.01 V... >>确定<<
27:VCC Target-7 (全部关闭) 0.00 V (0.00 至0.30)结果:0.01 V... >>确定<<
28:VCC Target-8 (全部关闭) 0.00 V (0.00 至0.30)结果:0.01 V... >>确定<<

29:转换器VT (关闭) 0.00 V (0.00 至0.50)结果:0.00 V... >>确定<<
30:转换器VT (1.8V) 1.80 V (1.60 至2.00)结果:0.05 V... >>错误<<
31:转换器VT (2.7V) 2.70 V (2.50 至2.90)结果:0.05 V... >>错误<<
32:转换VT (3.6V) 3.60 V (3.40 至3.80)结果:0.05 V ... >>错误<<

33:VPP电压- 10.00 V (8.00 至12.00)结果:10.08 V ... >>确定<<
34:VPP电压7.00 V (6.50 至7.30)结果:6.89 V ... >>确定<<
35:内部Vcc-3.3V 3.30 V (3.20 至3.40)结果:3.31 V ... >>确定<<

36:VCC Target-1 (全部在1.8V上) 1.80 V (1.60 至2.00)结果:1.80 V... >>确定<<
37:VCC Target-2 (全部为1.8V) 1.80 V (1.60 至2.00)结果:1.80 V... >>确定<<
38:VCC Target-3 (全部为1.8V) 1.80 V (1.60 至2.00)结果:1.79 V... >>确定<<
39:VCC Target-4 (全部为1.8V) 1.80 V (1.60 至2.00)结果:1.81 V... >>确定<<
40:VCC Target-5 (全部为1.8V) 1.80 V (1.60 至2.00)结果:1.80 V... >>确定<<
41:VCC Target-6 (全部为1.8V) 1.80 V (1.60 至2.00)结果:1.80 V... >>确定<<
42:VCC Target-7 (全部为1.8V) 1.80 V (1.60 至2.00)结果:1.80 V... >>确定<<
43:VCC Target-8 (全部为1.8V) 1.80 V (1.60 至2.00)结果:1.80 V... >>确定<<
44:VCC Target-1 (全部在2.7V上) 2.70 V (2.50 至2.90)结果:2.69 V... >>确定<<
45:VCC Target-2 (全部在2.7V上) 2.70 V (2.50 至2.90)结果:2.69 V... >>确定<<
46:VCC Target-3 (全部在2.7V上) 2.70 V (2.50 至2.90)结果:2.68 V... >>确定<<
47:VCC Target-4 (全部在2.7V上) 2.70 V (2.50 至2.90)结果:2.71 V... >>确定<<
48:VCC Target-5 (全部在2.7V上) 2.70 V (2.50 至2.90)结果:2.69 V... >>确定<<
49:VCC Target-6 (全部在2.7V上) 2.70 V (2.50 至2.90)结果:2.70 V... >>确定<<
50:VCC Target-7 (全部在2.7V上) 2.70 V (2.50 至2.90)结果:2.69 V... >>确定<<
51:VCC Target-8 (全部在2.7V上) 2.70 V (2.50 至2.90)结果:2.70 V... >>确定<<
52:VCC Target-1 (全部为3.6V) 3.60 V (3.40 至3.80)结果:3.58 V ... >>确定<<
53:VCC Target-2 (全部为3.6V) 3.60 V (3.40 至3.80)结果:3.59 V ... >>确定<<
54:VCC Target-3 (全部为3.6V) 3.60 V (3.40 至3.80)结果:3.58 V ... >>确定<<
55:VCC Target-4 (全部为3.6V) 3.60 V (3.40 至3.80)结果:3.61 V ... >>确定<<
56:VCC Target-5 (全部为3.6V) 3.60 V (3.40 至3.80)结果:3.59 V ... >>确定<<
57:VCC Target-6 (全部为3.6V) 3.60 V (3.40 至3.80)结果:3.60 V ... >>确定<<
58:VCC Target-7 (全部为3.6V) 3.60 V (3.40 至3.80)结果:3.59 V ... >>确定<<
59:VCC Target-8 (全部为3.6V) 3.60 V (3.40 至3.80)结果:3.61 V ... >>确定<<

60:VCC放电(100ms)目标-1 3.60 V (1.00 至2.70)结果:1.11 V... >>确定<<
61:VCC放电(100ms)目标-2 3.60 V (1.00 至2.70)结果:1.11 V... >>确定<<
62:VCC放电(100ms)目标-3 3.60 V (1.00 至2.70)结果:1.09 V... >>确定<<
63:VCC放电(100ms)Target-4 3.60 V (1.00 至2.70)结果:1.11 V... >>确定<<
64:VCC放电(100ms)Target-5 3.60 V (1.00 至2.70)结果:1.10 V... >>确定<<
65:VCC放电(100ms)Target-6 3.60 V (1.00 至2.70)结果:1.13 V... >>确定<<
66:VCC放电(100ms)Target-7 3.60 V (1.00 至2.70)结果:1.09 V... >>确定<<
67:VCC放电(100ms)Target-8 3.60 V (1.00 至2.70)结果:1.10 V... >>确定<<

68:VCC Target-1 (上的#1) 0.00 V (3.10 至3.50)结果:3.28 V... >>确定<<
69:VCC Target-2 (上的#1) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
70:VCC Target-3 (#1 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
71:VCC Target-4 (上的#1) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
72:VCC Target-5 (#1 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
73:VCC Target-6 (#1 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
74:VCC Target-7 (#1 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
75:VCC Target-8 (#1 ON) 3.30 V (0.00 至0.50)结果:0.14 V... >>确定<<
76:VCC Target-1 (2 ON) 0.00 V (0.00 至0.50)结果:0.15 V... >>确定<<
77:VCC Target-2 (#2 ON) 0.00 V (3.10 至3.50)结果:3.29 V... >>确定<<
78:VCC Target-3 (#2 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
79:VCC Target-4 (#2 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
80:VCC Target-5 (#2 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
81:VCC Target-6 (#2开) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
82:VCC Target-7 (#2 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
83:VCC Target-8 (#2 ON) 3.30 V (0.00 至0.50)结果:0.14 V... >>确定<<
84:VCC Target-1 (#3 ON) 0.00 V (0.00 至0.50)结果:0.15 V... >>确定<<
85:VCC Target-2 (#3 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
86:VCC Target-3 (#3 ON) 0.00 V (3.10 至3.50)结果:3.28 V... >>确定<<
87:VCC Target-4 (#3 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
88:VCC Target-5 (#3 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
89:VCC Target-6 (#3 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
90:VCC Target-7 (#3 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
91:VCC Target-8 (#3 ON) 3.30 V (0.00 至0.50)结果:0.14 V... >>确定<<
92:VCC Target-1 (#4 ON) 0.00 V (0.00 至0.50)结果:0.15 V... >>确定<<
93:VCC Target-2 (上的#4) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
94:VCC Target-3 (#4 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
95:VCC Target-4 (#4 ON) 0.00 V (3.10 至3.50)结果:3.30 V... >>确定<<
96:VCC Target-5 (#4 ON) 0.00 V (0.00 至0.50)结果:0.15 V... >>确定<<
97:VCC Target-6 (#4 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
98:VCC Target-7 (#4 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
99:VCC Target-8 (#4 ON) 3.30 V (0.00 至0.50)结果:0.14 V... >>确定<<
100:VCC Target-1 (5 ON) 0.00 V (0.00 至0.50)结果:0.15 V... >>确定<<
101:VCC Target-2 (上的#5) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
102:VCC Target-3 (#5 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
103:VCC Target-4 (5 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
104:VCC Target-5 (#5 ON) 0.00 V (3.10 至3.50)结果:3.29 V... >>确定<<
105:VCC Target-6 (#5 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
106:VCC Target-7 (#5 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
107:VCC Target-8 (5 ON) 3.30 V (0.00 至0.50)结果:0.14 V... >>确定<<
108:VCC Target-1 (#6 ON) 0.00 V (0.00 至0.50)结果:0.15 V... >>确定<<
109:VCC Target-2 (#6 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
110:VCC Target-3 (#6 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
111:VCC Target-4 (#6 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
112:VCC Target-5 (#6 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
113:VCC Target-6 (#6 ON) 0.00 V (3.10 至3.50)结果:3.29 V... >>确定<<
114:VCC Target-7 (#6 ON) 0.00 V (0.00 至0.50)结果:0.15 V... >>确定<<
115:VCC Target-8 (#6 ON) 3.30 V (0.00 至0.50)结果:0.14 V... >>确定<<
116:VCC Target-1 (上的#7) 0.00 V (0.00 至0.50)结果:0.15 V... >>确定<<
117:VCC Target-2 (上的#7) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
118:VCC Target-3 (#7 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
119:VCC Target-4 (#7 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
120:VCC Target-5 (#7 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
121:VCC Target-6 (上的#7) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
122:VCC Target-7 (#7 ON) 0.00 V (3.10 至3.50)结果:3.29 V... >>确定<<
123:VCC Target-8 (上的#7) 3.30 V (0.00 至0.50)结果:0.14 V... >>确定<<
124:VCC Target-1 (8 ON) 0.00 V (0.00 至0.50)结果:0.15 V... >>确定<<
125:VCC Target-2 (8 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
126:VCC Target-3 (8 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
127:VCC Target-4 (8 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
128:VCC Target-5 (8 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
129:VCC Target-6 (8 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
130:VCC Target-7 (8 ON) 0.00 V (0.00 至0.50)结果:0.14 V... >>确定<<
131:VCC Target-8 (8 ON) 3.30 V (3.10 至3.50)结果:3.30 V... >>确定<<

132:SD电源关闭0x0000 (0x0000 - 0x0000)结果:0x00... >>确定<<
133:SD电源开启0x0001 (0x0001 - 0x0001)结果:0x01 ... >>确定<<
134:SD放电-延迟2ms 0x0010 (0x0001 - 0x0001)结果:0x01 ... >>确定<<
135:SD放电-延迟50ms 0x0010 (0x0000 - 0x0000)结果:0x00... >>确定<<

136:BSL RX总线(#1高) 0x0001 (0x0001 - 0x0001)结果:0x00 ... >>错误<<
137:BSL RX总线(#2高) 0x0002 (0x0002 - 0x0002)结果:0x00... >>错误<<
138:BSL RX总线(#3高) 0x0004 (0x0004 - 0x0004)结果:0x00... >>错误<<
139:BSL RX总线(#4高) 0x0008 (0x0008 - 0x0008)结果:0x00... >>错误<<
140:BSL RX总线(#5高) 0x0010 (0x0010 - 0x0010)结果:0x00 ... >>错误<<
141:BSL RX总线(#6高) 0x0020 (0x0020 - 0x0020)结果:0x00 ... >>错误<<
142:BSL RX总线(#7高) 0x0040 (0x0040 - 0x0040)结果:0x00 ... >>错误<<
143:BSL RX总线(#8高) 0x0080 (0x0080 - 0x0080)结果:0x00 ... >>错误<<

144:BSL TX总线(#1高) 0x0001 (0x0001 - 0x0001)结果:0x00 ... >>错误<<
145:BSL TX总线(#2高) 0x0002 (0x0002 - 0x0002)结果:0x00... >>错误<<
146:BSL TX总线(#3高) 0x0004 (0x0004 - 0x0004)结果:0x00 ... >>错误<<
147:BSL TX总线(#4高) 0x0008 (0x0008 - 0x0008)结果:0x00... >>错误<<
148:BSL TX总线(#5高) 0x0010 (0x0010 - 0x0010)结果:0x00 ... >>错误<<
149:BSL TX总线(#6高) 0x0020 (0x0020 - 0x0020)结果:0x00 ... >>错误<<
150:BSL TX总线(#7高) 0x0040 (0x0040 - 0x0040)结果:0x00 ... >>错误<<
151:BSL TX总线(#8高) 0x0080 (0x0080 - 0x0080)结果:0x00 ... >>错误<<

152:TDI总线(#1高) 0x0001 (0x0001 - 0x0001)结果:0x00 ... >>错误<<
153:TDI总线(#2高) 0x0002 (0x0002 - 0x0002)结果:0x00... >>错误<<
154:TDI总线(#3高) 0x0004 (0x0004 - 0x0004)结果:0x00... >>错误<<
155:TDI总线(#4高) 0x0008 (0x0008 - 0x0008)结果:0x00... >>错误<<
156:TDI总线(#5高) 0x0010 (0x0010 - 0x0010)结果:0x00 ... >>错误<<
157:TDI总线(#6高) 0x0020 (0x0020 - 0x0020)结果:0x00 ... >>错误<<
158:TDI总线(#7高) 0x0040 (0x0040 - 0x0040)结果:0x00 ... >>错误<<
159:TDI总线(#8高) 0x0080 (0x0080 - 0x0080)结果:0x00 ... >>错误<<

160:TDOI Tx-bus (#1 high) 0x0001 (0x0001 - 0x0001)结果:0x00... >>错误<<
161:TDOI Tx-bus (#2 high ) 0x0002 (0x0002 - 0x0002)结果:0x00... >>错误<<
162:TDOI Tx-bus (#3 high ) 0x0004 (0x0004 - 0x0004)结果:0x00... >>错误<<
163:TDOI Tx-bus (#4 high ) 0x0008 (0x0008 - 0x0008)结果:0x00... >>错误<<
164:TDOI Tx-bus (#5 high ) 0x0010 (0x0010 - 0x0010)结果:0x00 ... >>错误<<
165:TDOI Tx-bus (#6 high ) 0x0020 (0x0020 - 0x0020)结果:0x00 ... >>错误<<
166:TDOI Tx-bus (#7 high ) 0x0040 (0x0040 - 0x0040)结果:0x00 ... >>错误<<
167:TDOI Tx-bus (#8 high ) 0x0080 (0x0080 - 0x0080)结果:0x00 ... >>错误<<

168:TDOI Tx-Rx (#1高) 0x0001 (0x0001 - 0x0001)结果:0xFF ... >>错误<<
169:TDOI Tx-Rx (#2高) 0x0002 (0x0002 - 0x0002)结果:0xFF ... >>错误<<
170:TDOI Tx-Rx (#3高) 0x0004 (0x0004 - 0x0004)结果:0xFF ... >>错误<<
171:TDOI Tx-Rx (#4高) 0x0008 (0x0008 - 0x0008)结果:0xFF ... >>错误<<
172:TDOI Tx-Rx (#5高) 0x0010 (0x0010 - 0x0010)结果:0xFF ... >>错误<<
173:TDOI Tx-Rx (#6高) 0x0020 (0x0020 - 0x0020)结果:0xFF ... >>错误<<
174:TDOI Tx-Rx (#7高) 0x0040 (0x0040 - 0x0040)结果:0xFF ... >>错误<<
175:TDOI Tx-Rx (#8高) 0x0080 (0x0080 - 0x0080)结果:0xFF ... >>错误<<

176:TDOI Rx-bus (#1 high) 0x0001 (0x0001 - 0x0001)结果:0x00 ... >>错误<<
177:TDOI Rx-bus (#2 high ) 0x0002 (0x0002 - 0x0002)结果:0x00... >>错误<<
178:TDOI Rx-bus (#3 high ) 0x0004 (0x0004 - 0x0004)结果:0x00... >>错误<<
179:TDOI Rx-bus (#4 high ) 0x0008 (0x0008 - 0x0008)结果:0x00... >>错误<<
180:TDOI Rx-bus (#5 high ) 0x0010 (0x0010 - 0x0010)结果:0x00 ... >>错误<<
181:TDOI Rx-bus (#6 high ) 0x0020 (0x0020 - 0x0020)结果:0x00 ... >>错误<<
182:TDOI Rx-bus (#7 high ) 0x0040 (0x0040 - 0x0040)结果:0x00 ... >>错误<<
183:TDOI Rx-bus (#84 high ) 0x0080 (0x0080 - 0x0080)结果:0x00 ... >>错误<<

184:TMS总线(全部高) 0x00FF (0x00FF - 0x00FF)结果:0x80... >>错误<<
185:TMS总线(全部为低) 0x0000 (0x0000 - 0x0000)结果:0x80... >>错误<<

186:TMS总线(#1高) 0x0001 (0x0001 - 0x0001)结果:0x00 ... >>错误<<
187:TMS总线(#2高) 0x0002 (0x0002 - 0x0002)结果:0x00... >>错误<<
188:TMS总线(#3高) 0x0004 (0x0004 - 0x0004)结果:0x00... >>错误<<
189:TMS总线(#4高) 0x0008 (0x0008 - 0x0008)结果:0x00 ... >>错误<<
190:TMS总线(#5高) 0x0010 (0x0010 - 0x0010)结果:0x00 ... >>错误<<
191:TMS总线(#6高) 0x0020 (0x0020 - 0x0020)结果:0x00 ... >>错误<<
192:TMS总线(#7高) 0x0040 (0x0040 - 0x0040)结果:0x00 ... >>错误<<
193:TMS总线(#8高) 0x0080 (0x0080 - 0x0080)结果:0x00 ... >>错误<<

194:RST总线(所有高) 0x00FF (0x00FF - 0x00FF)结果:0x00 ... >>错误<<
195:RST总线(全部为低) 0x0000 (0x0000 - 0x0000)结果:0x00... >>确定<<

196:RST总线(#1高) 0x0001 (0x0001 - 0x0001)结果:0x00 ... >>错误<<
197:RST总线(#2高) 0x0002 (0x0002 - 0x0002)结果:0x00... >>错误<<
198:RST总线(#3高) 0x0004 (0x0004 - 0x0004)结果:0x00 ... >>错误<<
199:RST总线(#4高) 0x0008 (0x0008 - 0x0008)结果:0x00 ... >>错误<<
200:RST总线(#5高) 0x0010 (0x0010 - 0x0010)结果:0x00 ... >>错误<<
201:RST总线(#6高) 0x0020 (0x0020 - 0x0020)结果:0x00 ... >>错误<<
202:RST总线(#7高) 0x0040 (0x0040 - 0x0040)结果:0x00 ... >>错误<<
203:RST总线(#8高) 0x0080 (0x0080 - 0x0080)结果:0x00 ... >>错误<<

204:密钥缓冲区(所有上拉) 0x001F (0x001F - 0x001F)结果:0x1f ... >>确定<<

205:访问LCD RAM (0xAA) 0x00AA (0x00AA - 0x00AA)结果:0xAA ... >>确定<<
206:访问LCD RAM (0x99) 0x0099 (0x0099 - 0x0099)结果:0x99 ... >>确定<<

207:映像快擦写访问(获取ID) 0x0002 (0x0001 - 0x0003)结果:0x01 ... >>确定<<

208:TDI保险丝键(#1开) 0x0001 (0x0001 - 0x0001)结果:0x00 ... >>错误<<
209:TDI保险丝键(#2打开) 0x0002 (0x0002 - 0x0002)结果:0x00 ... >>错误<<
210:TDI保险丝键(#3打开) 0x0004 (0x0004 - 0x0004)结果:0x00 ... >>错误<<
211:TDI保险丝键(#4打开) 0x0008 (0x0008 - 0x0008)结果:0x00... >>错误<<
212:TDI保险丝键(#5打开) 0x0010 (0x0010 - 0x0010)结果:0x00 ... >>错误<<
213:TDI Fuse keys (#6 on ) 0x0020 (0x0020 - 0x0020) result:0x00...(TDI保险丝键(#6打开) 0x0020 (0x0020 - 0x0020)结果:0x00 ... >>错误<<
214:TDI保险丝键(#7打开) 0x0040 (0x0040 - 0x0040)结果:0x00 ... >>错误<<
215:TDI保险丝键(#8开) 0x0080 (0x0080 - 0x0080)结果:0x00 ... >>错误<<

216:测试保险丝键(全部关闭) 0.00 (0.00 至0.30)结果:0.00 ... >>确定<<
217:测试保险丝钥匙(#1 ON) 1.00 (0.80 至3.00)结果:0.00 ... >>错误<<
218:测试保险丝钥匙(#2接通) 2.00 (0.80 至3.00)结果:0.00 ... >>错误<<
219:测试保险丝钥匙(#3接通) 3.00 (0.80 至3.00)结果:0.00 ... >>错误<<
220:测试保险丝钥匙(4号接通) 4.00 (0.80 至3.00)结果:0.00 ... >>错误<<
221:测试保险丝钥匙(#5接通) 5.00 (0.80 至3.00)结果:0.00 ... >>错误<<
222:测试保险丝钥匙(#6接通) 6.00 (0.80 至3.00)结果:0.00 ... >>错误<<
223:测试保险丝钥匙(#7接通) 7.00 (0.80 至3.00)结果:0.00 ... >>错误<<
224:测试保险丝钥匙(#8接通) 8.00 (0.80 至3.00)结果:0.00 ... >>错误<<

================= 已完成===========================================
*测试失败!! 86错误。
===================================================================================================================

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    这是一个常见的MSP-Gang MCU设备初始化错误:

    e2e.ti.com/.../38.7323万
    e2e.ti.com/.../63.2662万
    e2e.ti.com/.../20.5336万
    e2e.ti.com/.../56.4163万
    e2e.ti.com/.../63.4723万
    e2e.ti.com/.../56.9374万
    e2e.ti.com/.../36.0775万
    e2e.ti.com/.../28.3744万

    您的系统是否在工作状态和中断状态之间进行了任何更改? 您测试了多少台设备? 请检查您的电源,连接和接口选项。

    此致,
    Ryan
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    系统在工作状态和损坏状态之间没有变化,我测试了许多设备,更换了接头,使用了笔记本电脑的GUI界面或程序员的独立界面,但未解决问题。
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您使用的是TI EVM还是您自己的定制PCB? 您能否提供您的连接示意图? 您使用的是哪种接口?您是否能够使用示波器查看通信线路? GUI或LCD界面是否有任何其他错误详细信息? 日志似乎表明存在VT转换问题,但不清楚此电路是如何损坏的。

    此致,
    Ryan
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    首先,非常感谢您的帮助。  

    我使用的是定制印刷电路板,我们已经用相同的光化器对大约5000个印刷电路板进行了编程,但是编程器在一个好日子里就停止了工作。 请查找所附的PCB光绘数据的顶层和底层。 GUI或液晶屏上未显示其它错误。  VT转换问题,但不清楚此电路是如何损坏的,交流电压是否会造成任何损坏? 我检查了耙串分离器的针脚,但没有任何针脚电压。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    由于交流电压可能造成损坏,您应考虑获得另一个MSP组合以避免进一步延迟。

    此致,
    Ryan
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    没有其他选择? 任何维修方法?