This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430G2452:使用I2C在图形显示屏上显示文本

Guru**** 2614265 points
Other Parts Discussed in Thread: MSP430G2452

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/663984/msp430g2452-displaying-text-on-graphical-display-using-i2c

部件号:MSP430G2452

我尝试编写程序,通过I2C在图形LCD上显示一些数字(确切地说是DOGXL160-W)。 我设法清除和设置了显示屏上的所有像素,但当我尝试显示任何文本时,它要么不显示,要么代码太大,无法填充MSP430G2452。 我无法更改微控制器和LCD类型。 您能提供帮助吗?  

代码如下:  

无符号字符字体Int[]={/* USCI字体表7x5字体大小*/
0x00,0x00,0x00,0x00,0x00,0x00,0x00, /*每行描述7x5字体*/
0x00,0x00,0x00,0x00,0x00,0x00, /*一行中的每个元素描述7 (8)列像素*/
0x00,0x00,0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,0x00, 0x00,0x00,0x00,
0x00,0x00, 0x00,0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,0x00, 0x00,
0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
0x00, 0x00,0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,0x00, 0x00,0x00,
0x00,0x00,0x00, 0x00,0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00, 0xFE,0x00,0x00,0x00,0x00, 0xFE,0xFE,0x00,
0x00,0x00, 0xFE,0xFE,0xFE,0x00,0x00, 0xFE,0xFE,0xFE,0xFE,0x00, 0xFE,
0xFE,0xFE,0xFE,0xFE, 0x00,0xFE,0xFE,0xFE,0xFE, 0x00,0x00,0xFE,0xFE,
0xFE, 0x00,0x00,0x00,0xFE,0xFE, 0x00,0x00,0x00,0x00,0xFE, 0x06,0x0E,
0xFC,0x40,0x38, 0xC0,0xCC,0x12,0x12,0x12, 0xC0,0xDE,0x14,0x14,0x10,
0x20,0x30,0x38,0x30,0x20, 0x00,0x7C,0x38,0x10,0x00, 0x00,0x10,0x38,
0x7C,0x00, 0x08,0x18,0x38,0x18,0x08, 0x00,0x00,0x00,0x00,0x00, 0x00,
0x00,0xF2,0x00,0x00, 0x00,0xE0,0x00,0xE0,0x00, 0x28,0xFE,0x28,0xFE,
0x28, 0x24,0x54,0xFE,0x54,0x48, 0xc4,0xC8,0x10,0x26,0x46, 0x6C,0x92,
0xAA,0x44,0x0A, 0x00,0xA0,0xC0,0x00,0x00, 0x00,0x38,0x44,0x82,0x00,
0x00,0x82,0x44,0x38,0x00, 0x28,0x10,0x7C,0x10,0x28, 0x10,0x10,0x7C,
0x10,0x10, 0x00,0x0A,0x0C,0x00,0x00, 0x10,0x10,0x10,0x10,0x10, 0x00,
0x06,0x06,0x00,0x00, 0x04,0x08,0x10,0x20,0x40, 0x7C,0x8A,0x92,0xA2,
0x7C, 0x00,0x42,0xFE,0x02,0x00, 0x42,0x86,0x8A,0x92,0x62, 0x84,0x82,
0xA2,0xD2,0x8C, 0x18,0x28,0x48,0xFE,0x08, 0xE4,0xA2,0xA2,0xA2,0x9C,
0x3C,0x52,0x92,0x92,0x0C, 0x80,0x8E,0x90,0xA0,0xC0, 0x6C,0x92,0x92,
0x92,0x6C, 0x60,0x92,0x92,0x94,0x78, 0x00,0x6C,0x6C,0x00,0x00, 0x00,
0x6A,0x6C,0x00,0x00, 0x10,0x28,0x44,0x82,0x00, 0x28,0x28,0x28,0x28,
0x28, 0x00,0x82,0x44,0x28,0x10, 0x40,0x80,0x8A,0x90,0x60, 0x4C,0x92,
0x9E,0x82,0x7C, 0x7E,0x88,0x88,0x88,0x7E, 0xFE,0x92,0x92,0x92,0x6C,
0x7C,0x82,0x82,0x82,0x44, 0xFE,0x82,0x82,0x44,0x38, 0xFE,0x92,0x92,
0x92,0x82, 0xFE,0x90,0x90,0x90,0x80, 0x7C,0x82,0x92,0x92,0x5E, 0xFE,
0x10,0x10,0x10,0xFE, 0x00,0x82,0xFE,0x82,0x00, 0x04,0x02,0x82,0xFC,
0x80, 0xFE,0x10,0x28,0x44,0x82, 0xFE,0x02,0x02,0x02,0x02, 0xFE,0x40,
0x30,0x40,0xFE, 0xFE,0x20,0x10,0x08,0xFE, 0x7C,0x82,0x82,0x82,0x7C,
0xFE,0x90,0x90,0x90,0x60, 0x7C,0x82,0x8A,0x84,0x7A, 0xFE,0x90,0x98,
0x94,0x62, 0x62,0x92,0x92,0x92,0x8C, 0x80,0x80,0xFE,0x80,0x80, 0xFC,
0x02,0x02,0x02,0xFC, 0xf8,0x04,0x02,0x04,0xf8, 0xFC,0x02,0x1C,0x02,
0xFC, 0xC6,0x28,0x10,0x28,0xC6, 0xE0,0x10,0x0E,0x10,0xE0, 0x86,0x8A,
0x92,0xA2,0xC2, 0x00,0xFE,0x82,0x82,0x00, 0xA8,0x68,0x3E,0x68,0xA8,
0x00,0x82,0x82,0xFE,0x00, 0x20,0x40,0x80,0x40,0x20, 0x02,0x02,0x02,
0x02,0x02, 0x00,0x80,0x40,0x20,0x00, 0x04,0x2A,0x2A,0x2A,0x1E, 0xFE,
0x0A,0x12,0x12,0x0C, 0x1C,0x22,0x22,0x22,0x04, 0x0C,0x12,0x12,0x0A,
0xFE, 0x1C,0x2A,0x2A,0x2A,0x18, 0x10,0x7E,0x90,0x80,0x40, 0x30,0x4A,
0x4A,0x4A,0x7C, 0xFE,0x10,0x20,0x20,0x1E, 0x00,0x00,0x5E,0x00,0x00,
0x04,0x02,0x22,0xBC,0x00, 0xFE,0x08,0x14,0x22,0x00, 0x00,0x82,0xFE,
0x02,0x00, 0x3e,0x20,0x18,0x20,0x1E, 0x3e,0x10,0x20,0x20,0x1E, 0x1C,
0x22,0x22,0x22,0x1C, 0x3e,0x28,0x28,0x28,0x10, 0x10,0x28,0x28,0x18,
0x3E, 0x3e,0x10,0x20,0x20,0x10, 0x12,0x2A,0x2A,0x2A,0x04, 0x20,0xFC,
0x22,0x02,0x04, 0x3C,0x02,0x02,0x04,0x3E, 0x38,0x04,0x02,0x04,0x38,
0x3C,0x02,0x0C,0x02,0x3C, 0x22,0x14,0x08,0x14,0x22, 0x30,0x0A,0x0A,
0x0A,0x0A,0x3C, 0x22,0x26,0x2A,0x32,0x22, 0x00,0x10,0x6C,0x82,0x00, 0x00,
0x00,0xFE,0x00,0x00, 0x00,0x82,0x6C,0x10,0x00, 0x10,0x10,0x54,0x38,
0x10, 0x10,0x38,0x54,0x10,0x10, 0x0E,0x94,0x24,0x94,0x0E, 0x0E,0x14,
0xA4,0x14,0x0E, 0x0E,0x54,0xA4,0x54,0x0E, 0x04,0x2A,0x6A,0xAA,0x1E,
0x04,0x2A,0xAA,0x2A,0x1E, 0xFE,0xFE,0x92,0x92,0x92, 0xBC,0x42,0x42,
0x42,0xBC, 0x0C,0x52,0x12,0x52,0x0C, 0x3A,0x4C,0x54,0x64,0xB8, 0x18,
0x26,0x3C,0x64,0x18, 0xBC,0x02,0x02,0x02,0xBC, 0x1C,0x42,0x02,0x44,
0x1E, 0x40,0x20,0x10,0x08,0x04, 0x2A,0x2C,0x38,0x68,0xA8, 0x30,0x40,
0x30,0x08,0x30, 0x52,0xAA,0xAA,0xAA,0x94, 0x7E,0x90,0xFE,0x90,0x90,
0x2C,0x2A,0x1C,0x2A,0x1A, 0x12,0x7E,0x92,0x92,0x42, 0xFE,0xA0,0xA8,
0x5E,0x0A, 0x38,0x7C,0x7C,0x7C,0x38, 0x38,0x44,0x44,0x44,0x38, 0x10,
0x38,0x7C,0x38,0x10, 0x10,0x28,0x44,0x28,0x10, 0x00,0x00,0xEE,0x00,
0x00, 0x70,0x8A,0x8C,0x88,0x88, 0x06,0x0A,0x12,0x22,0x7E, 0x02,0x22,
0x52,0x8A,0x02, 0x02,0x8A,0x52,0x22,0x02, 0x08,0x1C,0x2A,0x08,0xf8,
0x20,0x40,0xFE,0x40,0x20, 0x08,0x04,0xFE,0x04,0x08, 0x00,0x00,0x00,
0x00,0x00, 0x0E,0x0A,0x0E,0x00,0x00, 0x00,0x00,0xF0,0x80,0x80, 0x02,
0x02,0x1E,0x00,0x00, 0x08,0x04,0x02,0x00,0x00, 0x00,0x18,0x18,0x00,
0x00, 0x50,0x50,0x52,0x54,0x78, 0x20,0x22,0x2C,0x28,0x30, 0x04,0x08,
0x1E,0x20,0x00, 0x18,0x10,0x32,0x12,0x1C, 0x12,0x12,0x1E,0x12,0x12,
0x12,0x14,0x18,0x3E,0x10, 0x10,0x3E,0x10,0x14,0x18, 0x02,0x12,0x12,
0x1E,0x02, 0x2A,0x2A,0x2A,0x3E,0x00, 0x18,0x00,0x1A,0x02,0x1C, 0x10,
0x10,0x10,0x10,0x10, 0x80,0x82,0xBC,0x90,0xE0, 0x08,0x10,0x3E,0x40,
0x80, 0x70,0x40,0xC2,0x44,0x78, 0x42,0x42,0x7E,0x42,0x42, 0x44,0x48,
0x50,0xFE,0x40, 0x42,0xFC,0x40,0x42,0x7C, 0x50,0x50,0xFE,0x50,0x50,
0x10,0x62,0x42,0x44,0x78, 0x20,0xC0,0x42,0x7C,0x40, 0x42,0x42,0x42,
0x42,0x7E, 0x40,0xF2,0x44,0xf8,0x40, 0x52,0x52,0x02,0x04,0x38, 0x42,
0x44,0x48,0x54,0x62, 0x40,0xFC,0x42,0x52,0x62, 0x60,0x12,0x02,0x04,
0x78, 0x10,0x62,0x52,0x4C,0x78, 0x50,0x52,0x7C,0x90,0x10, 0x70,0x00,
0x72,0x04,0x78, 0x20,0xA2,0xBC,0xA0,0x20, 0x00,0xFE,0x10,0x08,0x00,
0x22,0x24,0xf8,0x20,0x20, 0x02,0x42,0x42,0x42,0x02, 0x42,0x54,0x48,
0x54,0x60, 0x44,0x48,0xDE,0x68,0x44, 0x00,0x02,0x04,0xf8,0x00, 0x1E,
0x00,0x40,0x20,0x1E, 0xFC,0x22,0x22,0x22,0x22, 0x40,0x42,0x42,0x44,
0x78, 0x20,0x40,0x20,0x10,0x0C, 0x4C,0x40,0xFE,0x40,0x4C, 0x40,0x48,
0x44,0x4A,0x70, 0x00,0x54,0x54,0x54,0x02, 0x1C,0x24,0x44,0x04,0x0E,
0x02,0x14,0x08,0x14,0x60, 0x50,0x7C,0x52,0x52,0x52, 0x20,0xFE,0x20,
0x28,0x30, 0x02,0x42,0x42,0x7E,0x02, 0x52,0x52,0x52,0x52,0x7E, 0x20,
0xA0,0xA2,0xA4,0x38, 0xF0,0x02,0x04,0xf8,0x00, 0x3e,0x00,0x7E,0x02,
0x0C, 0x7E,0x02,0x04,0x08,0x10, 0x7E,0x42,0x42,0x42,0x7E, 0x70,0x40,
0x42,0x44,0x78, 0x42,0x42,0x02,0x04,0x18, 0x40,0x20,0x80,0x40,0x00,
0xE0,0xA0,0xE0,0x00,0x00, 0x1C,0x22,0x12,0x0C,0x32, 0x04,0xAA,0x2A,
0xAA,0x1E, 0x3e,0x54,0x54,0x54,0x28, 0x14,0x2A,0x2A,0x22,0x04, 0x7E,
0x08,0x08,0x10,0x78, 0x1C,0x22,0x32,0x2A,0x24, 0x1E,0x28,0x48,0x48,
0x30, 0x10,0x2A,0x2A,0x2A,0x3C, 0x04,0x02,0x3C,0x20,0x20, 0x40,0x40,
0x00,0xE0,0x00, 0x04,0x02,0x22,0xBC,0x00, 0xA0,0x40,0xA0,0x00,0x00,
0x18,0x24,0x7E,0x24,0x08, 0x28,0xFE,0x2A,0x02,0x02, 0x3e,0x90,0xA0,
0xA0,0x1E, 0x1C,0xA2,0x22,0xA2,0x1C, 0x7E,0x28,0x48,0x48,0x30, 0x30,
0x48,0x48,0x28,0x7E, 0x3C,0x52,0x52,0x52,0x3C, 0x0C,0x14,0x08,0x14,
0x18, 0x1A,0x26,0x20,0x26,0x1A, 0x3C,0x82,0x02,0x84,0x3E, 0xC6,0xAA,
0x92,0x82,0x82, 0x22,0x3C,0x20,0x3E,0x22, 0xA2,0x94,0x88,0x94,0xA2,
0x30,0x0A,0x0A,0x0A,0x0A,0x3C, 0x28,0x28,0x3E,0x28,0x48, 0x22,0x3C,0x28,
0x28,0x2E, 0x3e,0x28,0x38,0x28,0x3E, 0x10,0x10,0x54,0x10,0x10, 0x00,
0x00,0x00,0x00,0x00, 0xFE,0xFE,0xFE,0xFE,0xFE };


#include<MSP4S.h>

无效清除(无效)
{
无符号字符p;
无符号字符c;
无符号char sum, sumc;
I2C_Start();
(p = 0;p < 26;p++)
{/* 25页*/
(c = 0;c < 160;c++)
{/*160列*/
油底壳= 0x00 + p;
相扑= 0x00 + c;
setPageAddress (SE底壳);
setColumnAdress (相位);
I2C_OUT (0x00);
}
}
I2C_Stop();
}

void write (unsigned char row,unsigned char col,unsigned short f)
{ unsigned char LcdData[2];/*指向列*/的两页的指针
unsigned char *ptr;
无符号字符H = 0x00;
无符号字符L = 0x00;
无符号字符c;
(c = 0;c < 5;c++)
{/*字体块大小5列*/

L =(fontInt[f + c]和0x0F);/* LSB 4像素保存到L *
H =(fontInt[f + c]和0xF0);/* MSB 4像素保存到H *
H =(H >> 4);
LcdData[0]= 0x00;
LcdData[1]= 0x00;
如果((H和0x01)= 0x01)
{/* H中的每个像素被转换为2位,11像素开- 00像素关*/
LcdData[0]= LcdData[0]+ 0xC0;
};

如果((H和0x02)= 0x02)
{
LcdData[0]= LcdData[0]+ 0x30;
};

如果((H和0x04)= 0x04)
{
LcdData[0]= LcdData[0]+ 0x0C;
};

如果((H和0x08)= 0x08)
{
LcdData[0]= LcdData[0]+ 0x03;
};

如果(L和0x01)= 0x01)
{/* L中的每个像素被转换为2位,11像素开- 00像素关*/
LcdData[1]= LcdData[1]+0xC0;
};

如果(L和0x02)= 0x02)
{
LcdData[1]= LcdData[1]+0x30;
};

如果(L和0x04)= 0x04)
{
LcdData[1]= LcdData[1]+0x0C;
};

如果(L和0x08)== 0x08)
{
LcdData[1]= LcdData[1]+0x03;
};
unsigned char p,Setp,SETC;
(p = 0;p < 2;p++)
{/*字体页大小2页*/
PTR = LcdData + p;
Setp = 0x00 + p +行;
setPageAddress (设置);

SETC = 0x00 + c + col;
setColumnAdress (SETC);

I2C_OUT (* PTR);/*由两个页面组成的列被发送到LCD */
}
}
}

void setPageAddress (无符号字符PA)
{
unsigned char Cmd = 0x60 + pa;/*页面地址命令=页面地址初始命令+页面地址*/
I2C_Start();
I2C_OUT (Cmd);
I2C_Stop();
}

void setColumnAdress (unsigned char CA)
{
无符号字符H = 0x00;
无符号字符L = 0x00;
无符号字符列地址[]={ 0x00, 0x10};
L =(CA和0x0F);/*单独命令降级为低和高*/
H =(CA和0xF0);
H =(H >> 4);
ColumnAddress[0]=(0x00 + L);/*列地址CommandLSB =列地址初始命令*/
/*+列地址位0..3*/
ColumnAddress[1]=(0x10 + H);/*列地址CommandMSB =列地址初始命令*/
/*+列地址位4..7*/
I2C_Start();
I2C_OUT (ColumnAddress[0]);
I2C_OUT (ColumnAddress[1]);
I2C_Stop();
}

void writeString(unsigned char y, unsigned char x, char word[])
{
无符号字符k;
无符号字符A =0;

做
{/*将字体写入8x5像素*/块
K =单词[A];
写入(y,x,5 * k);
x = x + 6;/*指向下一个块*/
A+++;
K =单词[A];
}
而(k !=0);/*写入到字符串*/
}/*末尾

的是粗略延迟函数。 通过更改计数器值进行调整。 */
void delay (无符号int n)
{
易失性int I;

用于(; n; n--)
{
(i = 0;i < 50;I++)
;}

}

void data_read(void){

P1DIR ==~I2C_SDA;// float以准备读取
}

void data_high (void)
{
P1DIR &=~I2C_SDA;//浮子引脚进入高位
DELAY (5);
}

void data_low(void)
{
P1OUT &=~I2C_SDA;//断言低
P1DIR |= I2C_SDA;
DELAY (5);
}

void clk_high (void)
{
P1DIR &=~I2C_SCL;//浮子引脚进入高位
delay(10);
}

void clk_low(void){

P1OUT &=~I2C_SCL;//断言低
P1DIR |= I2C_SCL;
DELAY (5);
}/*

I2C通信在数据
和时钟*线路均以该顺序低电平时开始。 */
void I2C_Start (void)
{
clk_high ();
DATA_HIGH ();
DATA_low();
clk_low();
}/*

I2C通信停止,时钟
和数据*线路按该顺序都高。 */
void I2C_Stop (void)
{
DATA_low();
clk_low();
clk_high ();
DATA_HIGH ();
}/*

通过I2C线路输出8位命令或数据。 */
void I2C_OUT (无符号字符d)
{
int n;

(n = 0;n < 8;n++)
{
如果(D和0x80)
{
DATA_HIGH ();
}
否则
{
DATA_low();}


clk_high ();
clk_low();

d <<= 1; //将下一位移动到位
。}

data_read(); //设置要接收的数据行。
clk_high (); //时钟变高以等待确认。

//从属设备将拉低数据线以确认。
While (P1IN和I2C_SDA)
{
//否则切换时钟线并再次检查
clk_low();
clk_high ();
}

clk_low();
}/*

初始化LCD面板。 */
void init_lcd (void)
{
I2C_Start();

I2C_OUT (0xF1);//com end
I2C_OUT (0x67);//
I2C_OUT (0xC0);//映射控制
I2C_OUT (0x40);//滚动线lsb
I2C_OUT (0x50);//滚动行MSB
I2C_OUT (0x2B);//设置面板加载
I2C_OUT (0xEB);//设置LCD偏置比
I2C_OUT (0x81);//设置vbias电位计
I2C_OUT (0x5F);//
I2C_OUT (0x89);//设置ram地址控制
I2C_OUT (0xAF);//设置显示启用
延迟(10);

I2C_Stop();
}

void reset()
{
I2C_Start();
I2C_OUT (0xE2);
I2C_Stop();
}

void allPixelsOn()
{
I2C_Start();
I2C_OUT (0xA5);
I2C_Stop();
}

int main(void)
{

/*停止看门狗计时器,使其不会重置芯片*/
WDTCTL = WDTPW + WDTHOLD;

INIT_LCD();

I2C_Start();

Clear();
writeString (10,50,"12");
I2C_Stop();

// allPixelsOn();

__bis_sr_register( LPM3_bits);/*进入睡眠*/
} 

字体和部分代码来自EA提供的应用说明(https://www.lcd-module.com/support/application-note.html

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Toann,您好!

    让我来澄清您的问题:您正在尝试使用MSP430G2452通过I2C在图形LCD上显示数字。 据我所知,您不确定文本是否未显示,或者代码大小是否不适合MSP430G2452内存。

    您是否收到代码大小过大的通知? 您可以在使用的IDE中通过查看内存分配来检查此问题。 生成项目时,链接器应警告您,您的代码大小也不能在内存中容纳。 否则应该没问题。

    正如您所提到的,您可以处理清除和设置所有像素的问题,我认为您的I2C通信工作正常,只是为了确保您可以查看 我们的MSP430TmMCU上常见eUSCI和USCI串行通信问题解决方案 应用报告。

    EA应用程序说明包括LCD初始化与清除/写入之间的延迟。 您是否在开始写入时检查了液晶屏是否就绪?

    您也可以尝试 先显示单个数字或字符,以查看是否有效。

    如果有任何提示可以帮助您,请告诉我,同时我将进一步了解您的代码。

    此致,

    Britta Ruelander

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Britta,

    感谢您的关注。  

    是的,我尝试使用MSP430G2452通过I2C在图形LCD上显示数字。 昨天,代码大小不适合MSP430G2452内存,我收到错误“程序不适合可用内存,运行区域定位失败...”,但我建立了数组“fontyInt”连接,现在它适合,但不起作用。  

    我也不确定I2C通信是否正常工作,实际上我认为不是-我一定把背光错误地"设置为所有像素打开",我认为我关闭了(我知道,这是一个基本的愚蠢错误)。 我将在应用报告中查看解决方案。  

    我尝试增加不同长度的延迟,没有任何改变。 如何检查液晶屏是否就绪?  

    我尝试显示单个数字,但没有发生。  

    Toann

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    Toann,您好!

    感谢您的澄清。
    我建议您首先尝试验证I2C通信是否正常工作。 希望我建议的应用报告能够帮助您。 您可能希望尝试通过使用示波器进行调试和监控来验证I2C消息。

    如果这有助于I2C通信正常工作,请告诉我。

    此致,
    Britta Ruelander
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    好的,我设法使I2C通信正常工作。 初始化显示器后,我可以设置其上的所有像素或重置显示器,但我无法写入任何特定内容(如数字)。 请你给我一些建议吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您好,

    很高兴听到I2C通信正在工作。

    对我来说,您的问题听起来像是显示问题,而不是MSP方面的问题,因此我没有详细信息。
    但是,一个常见的问题是,您正在对实际显示之外的像素进行索引(例如,因为您使用的是显示系列中较小的显示)。 这样,您的命令将是正确的,但您不会在显示屏上看到任何更改。

    我建议您联系显示器供应商寻求支持,因为他们了解所有细节,希望能立即为您提供帮助。

    此致,
    Britta.
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您好,
    这就是我要做的。 谢谢!
    此致。
    Toann