This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CCS/MSP430F5438A:信道序列

Guru**** 2610575 points
Other Parts Discussed in Thread: MSP430F5438A

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/661777/ccs-msp430f5438a-sequence-of-channels

部件号:MSP430F5438A

工具/软件:Code Composer Studio

您好,

我正在为学校做一个项目,我需要帮助。
我们正在使用MSP430F5438A微控制器和Code Composer Studio v7。
我们需要编写一个程序来读取两个电压通道(ADC14和ADC15)并在LCD显示屏上显示这些值。  采集和采样频率控制的开始使用S1–S4按键完成。 采样频率的范围可以从0.5 到5 Hz不等。

我们也得到了
数据表(http://www.ti.com/lit/ds/symlink/msp430f5438a.pdf)
用户指南(http://www.ti.com/lit/ug/slau208p/slau208p.pdf)


我需要有关频道顺序模式的帮助。

提前感谢您的帮助。
Milica