This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR5.9941万:在错误模式下切换复位引脚的器件不会退出,但在切断电源并重新应用后,器件能够正常运行

Guru**** 2507255 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1096940/msp430fr59941-device-in-error-mode-which-toggling-the-reset-pin-does-not-take-out-of-but-after-cutting-power-and-reapplying-device-was-able-to-operate-normally

部件号:MSP430FR5.9941万

我们有 一个MSP430FR5.9941万,它连接到另一个微控制器,控制连接 到MSP430FR5.9941万的重置线路,MSP430进入了某种错误状态,芯片没有响应,因此连接的微控制器尝试将重置引脚保持在低电平50多us的状态,以使MSP430恢复。 但无法重置MSP430。 我通过示波器确认重置线路确实是低到高,我们甚至尝试手动将线路短接至GND以使MSP430重置,但MSP430仍然没有响应。 在切断MSP430的电压并重新施加电压后,MSP430能够对重置引脚作出响应并做出正确反应(尽管我们迄今为止一直无法重现先前的错误状态)。 我的问题是:是否存在MSP430无法响应重置线路而需要关闭电源以进行重置的情况?